This is an old revision of the document!
This page offers product-specific organization of the video tutorials. Use the Table of Contents to quickly access the products of interest.
Internet Explorer users will want to make sure that Protected Mode has been diabled before clicking on any of these links.
Starting at the Menu Bar at the top of the Internet Explorer screen, use the following click path to access the Protected Mode check box: Tools > Internet Options > Security.
If you must click on the box to disable it, make sure to click on Apply before clicking on OK to exit the Internet Options menu.
Click on the video titles to directly access the video tutorial files. When there is only a title, that indicates that this video is in planning or production, but will be available in the near future.
TITLE/LINK | TYPE | DURATION | SUMMARY |
---|---|---|---|
IMU Evaluation Tools and Online Information | MP4 | 3m:39s | Starting at the home page, observe step-by-step instruction on how to quickly identify the right evaluation tools, along with setup and common use information. |
IMU Datasheets; How can they help me? | MP4 | 4m:12s | Take a quick journey through the ADIS16485 datasheet to find out where to locate answers to the 13 most common questions that engineers have when designing with these products. |
IMU Design Tools on the Web | MP4 | 2m:32s | Watch this video to find out where we hide key design tools, such as PCB CAD libraries, 3-D Models, Code examples, etc. |
IMU Performance Optimization, The Basics | |||
IMU Mounting for Optimal Bias Repeatability | |||
IMU Connection, Tips for Quick SPI Success | |||
Measuring Total Noise on the EVAL-ADIS | |||
Measuring Noise Density on the EVAL-ADIS | |||
Measuring Angle Random Walk (ARW) on the EVAL-ADIS | |||
Measuring In-run bias stability on the EVAL-ADIS | |||
Measuring Scale Factor/Sensitivity on the EVAL-ADIS | |||
Measuring Alignment Error on the EVAL-ADIS | |||
Inertial test platform communications | |||
VIDEO TITLE/LINK | SUMMARY |
---|---|
Writing to Registers | Register read and write examples, using Register Access menu. |
Manual FFT Mode Demonstration | Manual FFT mode example that uses the Main Window drop-down selector and illustrates the resulting register (REC_CTRL1) changes in the Register Access menu. |
Automatic FFT Mode Demonstration | |
Sample Rate Control Demonstration | |
Automated Offset Correction Demonstration | |
Manual FFT/Multi-Record Demonstration | |
Automatic FFT/Multi-Record Demonstration | |
Alarm Demonstration | |
Data Capture Demonstration & FFT Header Explanation |