Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:inertial-mems:imu:adis16imu2-pcb [01 Dec 2017 20:51] – [INTERFACE CONNECTORS] Mark Looney | resources:eval:user-guides:inertial-mems:imu:adis16imu2-pcb [19 Oct 2023 17:52] (current) – [GENERAL DESCRIPTION] Mark Looney |
---|
====== ADIS16IMU2/PCBZ Breakout Board Wiki-Guide ====== | ====== ADIS16IMU2/PCBZ Breakout Board Wiki-Guide ====== |
| =====GENERAL DESCRIPTION===== |
| The ADIS16IMU2/PCBZ is a breakout board that provides the ability to connect with the following products, using a standard ribbon cable (16-pin, 1mm pitch): [[adi>ADIS16334|ADIS16334]], [[adi>ADIS16362|ADIS16362]], [[adi>ADIS16364|ADIS16364]], [[adi>ADIS16365|ADIS16365]], [[adi>ADIS16367|ADIS16367]], [[adi>ADIS16405|ADIS16405]], [[adi>ADIS16407|ADIS16407]], [[adi>ADIS16445|ADIS16445]]. This breakout board simplifies connection to an embedded processor system, early in the development cycle and also connects this products to the [[adi>EVAL-ADIS-FX3|EVAL-ADIS-FX3]] or EVAL-ADIS2 (obsolete) evaluation systems. |
| |
| {{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_pcb_00.jpg?200|}} |
| |
| |
| |
| |
| =====SETUP WITH ADIS1633X/44X IMUS===== |
=====SETUP WITH ADIS16334 & ADIS1644x IMUS===== | |
Connecting the IMU (ADIS16334, ADIS16445 or ADIS16448), ADIS1644X/FLEX and ADIS16IMU2 together is a very simple two-step process. Please note that the pin numbers markings on the ADIS1644X/FLEX were incorrect in early manufacturing lots. Please ignore the pin number markings on the ADIS1644X/FLEX and use the following instructions to guide the connection process. | Connecting the IMU (ADIS16334, ADIS16445 or ADIS16448), ADIS1644X/FLEX and ADIS16IMU2 together is a very simple two-step process. Please note that the pin numbers markings on the ADIS1644X/FLEX were incorrect in early manufacturing lots. Please ignore the pin number markings on the ADIS1644X/FLEX and use the following instructions to guide the connection process. |
| |
| |
{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_adis1644x_flex_02.png?500|}} | {{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_adis1644x_flex_02.png?500|}} |
| |
<WRAP alert>**WARNING!** The connector pin numbers on the ADIS1644X/FLEX do not match the pin assignments on the DUT (ADIS1633x or ADIS1644x) or breakout board (ADIS16IMU2/PCBZ). Do not use these markings to determine proper connector alignment. Use the diagrams in this Wiki Guide to determine proper pin alignment with the DUT and breakout board.</WRAP> | |
| |
The following diagram shows the IMU's interface connector, which the ADIS1644X/FLEX connects with: | The following diagram shows the IMU's interface connector, which the ADIS1644X/FLEX connects with: |
| |
| |
| =====SETUP WITH ADIS1636x/40X IMUs===== |
| Connecting any of the ADIS1636x or ADIS1640x IMU products is very simple, as J2 mates perfectly with the interface connect on these products. Click on any of the images to below for larger views. |
| ^ ^ ^ ^ ^ |
| |{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wikiguide_adis1640x_install_00.png?360|}} |{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wikiguide_adis1640x_install_01.png?400|}}| |
| |
| |{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wikiguide_adis1640x_install_02.png?440|}} |{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wikiguide_adis1640x_install_04.png?400|}}| |
| |
| For more information on proper handling of the ADIS1636x and ADIS1640x packages, please consult [[adi>media/en/technical-documentation/application-notes/AN-1045.pdf|AN-1045]] |
| =====KEY PHYSICAL DIMENSIONS===== |
| Please see the following diagram for dimensions of all key physical attributes: |
| |
| {{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_pcb_dimensions.png?300|}} |
| |
| |
| =====INTERFACE CONNECTOR===== |
| J1 is the electrical connector that provides direct access to power, ground and critical digital I/O pins on the devices. It is a 16-pin, dual-row, 2-mm pitch connector that support 1mm ribbon cable systems. |
| |
| ===Pin Assignments=== |
| |
| Here is the pin assignments for J1, which is the connector that will interface with an embedded processor board. |
| |
| {{:resources:eval:user-guides:inertial-mems:imu:adis16imu1-pcb-j1-connector.png?200|}} |
| |
| ===Ribbon Cable Options=== |
| Check out the following link for ideas on how to make or purchase 16-pin, 1mm ribbon cables that can mate to the ADIS16IMU2/PCBZ. |
| |
| [[ez>docs/DOC-2523|Acquiring 1mm ribbon cables]] |
| |
| =====ELECTRICAL SCHEMATIC====== |
| |
| {{:resources:eval:user-guides:inertial-mems:imu:adis16imu1-pcb-schematic.png?400|}} |
| |
=====SUPPORT===== | =====SUPPORT===== |