Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:inertial-mems:imu:adis16imu2-pcb [01 Dec 2017 16:59] – [ELECTRICAL SCHEMATIC] Mark Looney | resources:eval:user-guides:inertial-mems:imu:adis16imu2-pcb [19 Oct 2023 17:52] (current) – [GENERAL DESCRIPTION] Mark Looney |
---|
====== ADIS16IMU2/PCBZ Breakout Board Wiki-Guide ====== | ====== ADIS16IMU2/PCBZ Breakout Board Wiki-Guide ====== |
=====GENERAL DESCRIPTION===== | =====GENERAL DESCRIPTION===== |
The ADIS16IMU2/PCBZ is a breakout board that provides the ability to connect with the following products, using a standard ribbon cable (16-pin, 1mm pitch): [[adi>ADIS16334|ADIS16334]], [[adi>ADIS16362|ADIS16362]], [[adi>ADIS16364|ADIS16364]], [[adi>ADIS16365|ADIS16365]], [[adi>ADIS16367|ADIS16367]], [[adi>ADIS16405|ADIS16405]], [[adi>ADIS16407|ADIS16407]], [[adi>ADIS16445|ADIS16445]]. This breakout board simplifies connection to an embedded processor system, early in the development cycle and also connects this products to the EVAL-ADIS2 evaluation system. | The ADIS16IMU2/PCBZ is a breakout board that provides the ability to connect with the following products, using a standard ribbon cable (16-pin, 1mm pitch): [[adi>ADIS16334|ADIS16334]], [[adi>ADIS16362|ADIS16362]], [[adi>ADIS16364|ADIS16364]], [[adi>ADIS16365|ADIS16365]], [[adi>ADIS16367|ADIS16367]], [[adi>ADIS16405|ADIS16405]], [[adi>ADIS16407|ADIS16407]], [[adi>ADIS16445|ADIS16445]]. This breakout board simplifies connection to an embedded processor system, early in the development cycle and also connects this products to the [[adi>EVAL-ADIS-FX3|EVAL-ADIS-FX3]] or EVAL-ADIS2 (obsolete) evaluation systems. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_pcb_00.jpg?200|}} | {{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_pcb_00.jpg?200|}} |
| |
| |
=====SETUP WITH ADIS16334 & ADIS1644x IMUS===== | =====SETUP WITH ADIS1633X/44X IMUS===== |
Connecting the IMU (ADIS16334, ADIS16445 or ADIS16448), ADIS1644X/FLEX and ADIS16IMU2 together is a very simple two-step process. Please note that the pin numbers markings on the ADIS1644X/FLEX were incorrect in early manufacturing lots. Please ignore the pin number markings on the ADIS1644X/FLEX and use the following instructions to guide the connection process. | Connecting the IMU (ADIS16334, ADIS16445 or ADIS16448), ADIS1644X/FLEX and ADIS16IMU2 together is a very simple two-step process. Please note that the pin numbers markings on the ADIS1644X/FLEX were incorrect in early manufacturing lots. Please ignore the pin number markings on the ADIS1644X/FLEX and use the following instructions to guide the connection process. |
| |
| |
{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_adis1644x_flex_02.png?500|}} | {{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_adis1644x_flex_02.png?500|}} |
| |
<WRAP alert>**WARNING!** The connector pin numbers on the ADIS1644X/FLEX do not match the pin assignments on the ADIS1633x, ADIS1644x IMUs or ADIS16IMU2/PCBZ breakout boards.</WRAP> | |
| |
The following diagram shows the IMU's interface connector, which the ADIS1644X/FLEX connects with: | The following diagram shows the IMU's interface connector, which the ADIS1644X/FLEX connects with: |
For more information on proper handling of the ADIS1636x and ADIS1640x packages, please consult [[adi>media/en/technical-documentation/application-notes/AN-1045.pdf|AN-1045]] | For more information on proper handling of the ADIS1636x and ADIS1640x packages, please consult [[adi>media/en/technical-documentation/application-notes/AN-1045.pdf|AN-1045]] |
=====KEY PHYSICAL DIMENSIONS===== | =====KEY PHYSICAL DIMENSIONS===== |
Please see the following diagram for dimensions of the key physical attributes in the ADIS1644X/FLEX: | Please see the following diagram for dimensions of all key physical attributes: |
| |
COMING SOON.... | {{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_pcb_dimensions.png?300|}} |
| |
| |
=====INTERFACE CONNECTORS===== | =====INTERFACE CONNECTOR===== |
| J1 is the electrical connector that provides direct access to power, ground and critical digital I/O pins on the devices. It is a 16-pin, dual-row, 2-mm pitch connector that support 1mm ribbon cable systems. |
COMING SOON..... | |
| |
===Pin Assignments=== | ===Pin Assignments=== |
| |
COMING SOON.... | Here is the pin assignments for J1, which is the connector that will interface with an embedded processor board. |
| |
| {{:resources:eval:user-guides:inertial-mems:imu:adis16imu1-pcb-j1-connector.png?200|}} |
| |
===Ribbon Cable Options=== | ===Ribbon Cable Options=== |
=====ELECTRICAL SCHEMATIC====== | =====ELECTRICAL SCHEMATIC====== |
| |
COMING SOON.... | {{:resources:eval:user-guides:inertial-mems:imu:adis16imu1-pcb-schematic.png?400|}} |
| |
=====SUPPORT===== | =====SUPPORT===== |