Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:inertial-mems:imu:adis16imu2-pcb [23 Dec 2016 22:49] – [SUMMARY] Mark Looney | resources:eval:user-guides:inertial-mems:imu:adis16imu2-pcb [19 Oct 2023 17:52] (current) – [GENERAL DESCRIPTION] Mark Looney |
---|
====== ADIS16IMU2/PCBZ Breakout Board Wiki-Guide ====== | ====== ADIS16IMU2/PCBZ Breakout Board Wiki-Guide ====== |
=====GENERAL DESCRIPTION===== | =====GENERAL DESCRIPTION===== |
The ADIS16IMU2/PCBZ is a breakout board that provides the ability to connect with the following products, using a standard ribbon cable (16-pin, 1mm pitch): [[adi>ADIS16334|ADIS16334]], [[adi>ADIS16362|ADIS16362]], [[adi>ADIS16364|ADIS16364]], [[adi>ADIS16365|ADIS16365]], [[adi>ADIS16367|ADIS16367]], [[adi>ADIS16405|ADIS16405]], [[adi>ADIS16407|ADIS16407]], [[adi>ADIS16445|ADIS16445]]. This breakout board simplifies connection to an embedded processor system, early in the development cycle and also connects this products to the EVAL-ADIS2 evaluation system. | The ADIS16IMU2/PCBZ is a breakout board that provides the ability to connect with the following products, using a standard ribbon cable (16-pin, 1mm pitch): [[adi>ADIS16334|ADIS16334]], [[adi>ADIS16362|ADIS16362]], [[adi>ADIS16364|ADIS16364]], [[adi>ADIS16365|ADIS16365]], [[adi>ADIS16367|ADIS16367]], [[adi>ADIS16405|ADIS16405]], [[adi>ADIS16407|ADIS16407]], [[adi>ADIS16445|ADIS16445]]. This breakout board simplifies connection to an embedded processor system, early in the development cycle and also connects this products to the [[adi>EVAL-ADIS-FX3|EVAL-ADIS-FX3]] or EVAL-ADIS2 (obsolete) evaluation systems. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_pcb_00.jpg?200|}} | {{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_pcb_00.jpg?200|}} |
Connecting any of the ADIS1636x or ADIS1640x IMU products is very simple, as J2 mates perfectly with the interface connect on these products. Click on any of the images to below for larger views. | Connecting any of the ADIS1636x or ADIS1640x IMU products is very simple, as J2 mates perfectly with the interface connect on these products. Click on any of the images to below for larger views. |
^ ^ ^ ^ ^ | ^ ^ ^ ^ ^ |
|{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wikiguide_adis1640x_install_00.png?180|}} |{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wikiguide_adis1640x_install_01.png?200|}} |{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wikiguide_adis1640x_install_02.png?220|}} |{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wikiguide_adis1640x_install_04.png?200|}}| | |{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wikiguide_adis1640x_install_00.png?360|}} |{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wikiguide_adis1640x_install_01.png?400|}}| |
| |
| |{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wikiguide_adis1640x_install_02.png?440|}} |{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wikiguide_adis1640x_install_04.png?400|}}| |
| |
For more information on proper handling of the ADIS1636x and ADIS1640x packages, please consult [[adi>media/en/technical-documentation/application-notes/AN-1045.pdf|AN-1045]] | For more information on proper handling of the ADIS1636x and ADIS1640x packages, please consult [[adi>media/en/technical-documentation/application-notes/AN-1045.pdf|AN-1045]] |
| =====KEY PHYSICAL DIMENSIONS===== |
| Please see the following diagram for dimensions of all key physical attributes: |
| |
| {{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_pcb_dimensions.png?300|}} |
| |
| |
=====INTERFACE CONNECTOR===== | =====INTERFACE CONNECTOR===== |
J1 is the electrical connector that provides direct access to power, ground and critical digital I/O pins on the devices. It is a 16-pin, dual-row, 2-mm pitch connector that support 1mm ribbon cable systems. | J1 is the electrical connector that provides direct access to power, ground and critical digital I/O pins on the devices. It is a 16-pin, dual-row, 2-mm pitch connector that support 1mm ribbon cable systems. |