Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
resources:eval:user-guides:inertial-mems:imu:adis16imu2-pcb [19 Apr 2016 19:23] – [SETUP WITH ADIS1636x/40X IMUs] Mark Looney | resources:eval:user-guides:inertial-mems:imu:adis16imu2-pcb [23 Dec 2016 22:49] – [SUMMARY] Mark Looney |
---|
====== ADIS16IMU2/PCBZ Breakout Board Wiki-Guide ====== | ====== ADIS16IMU2/PCBZ Breakout Board Wiki-Guide ====== |
=====GENERAL DESCRIPTION===== | =====GENERAL DESCRIPTION===== |
The ADIS16IMU2/PCBZ is a breakout board that provides some convenience for those who are connecting an [[adi>ADIS16334|ADIS16334]], [[adi>ADIS16362|ADIS16362]], [[adi>ADIS16364|ADIS16364]], [[adi>ADIS16365|ADIS16365]], [[adi>ADIS16367|ADIS16367]], [[adi>ADIS16405|ADIS16405]], [[adi>ADIS16407|ADIS16407]], [[adi>ADIS16445|ADIS16445]] and [[adi>ADIS16448|ADIS16448]] to an embedded processor for the first time. | The ADIS16IMU2/PCBZ is a breakout board that provides the ability to connect with the following products, using a standard ribbon cable (16-pin, 1mm pitch): [[adi>ADIS16334|ADIS16334]], [[adi>ADIS16362|ADIS16362]], [[adi>ADIS16364|ADIS16364]], [[adi>ADIS16365|ADIS16365]], [[adi>ADIS16367|ADIS16367]], [[adi>ADIS16405|ADIS16405]], [[adi>ADIS16407|ADIS16407]], [[adi>ADIS16445|ADIS16445]]. This breakout board simplifies connection to an embedded processor system, early in the development cycle and also connects this products to the EVAL-ADIS2 evaluation system. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_pcb_00.jpg?200|}} | {{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_pcb_00.jpg?200|}} |
| |
=====SUMMARY===== | |
When used in conjunction with the ADIS1644X/FLEX, the ADIS16IMU2/PCBZ can connect the ADIS16334, ADIS16445 or ADIS16448 to the EVAL-ADIS or to an embedded processor system. Please see the following picture, which illustrates how each of these components fit together: | |
| |
{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_functional_00.jpg?600|}} | |
| |
=====ADIS1644X/FLEX PIN NUMBER MARKINGS===== | |
Please note that the pin numbers markings on the ADIS1644X/FLEX were incorrect in early manufacturing lots. The following picture illustrates the corrected pin numbers. This picture is here to raise awareness and to recommend that these pin numbers be ignored, in deference to the following procedure for correct installation (which does not require reference to these pin number markings): | |
| |
{{:resources:eval:user-guides:inertial-mems:imu:ez_faq_adis16448_flex_incorrectpinnumbers_01.png?500|}} | |
| |
=====SETUP WITH ADIS1633X/44X IMUS===== | =====SETUP WITH ADIS1633X/44X IMUS===== |
Connecting the IMU (ADIS16334, ADIS16445 or ADIS16448), ADIS1644X/FLEX and ADIS16IMU2 together is a very simple two-step process. | Connecting the IMU (ADIS16334, ADIS16445 or ADIS16448), ADIS1644X/FLEX and ADIS16IMU2 together is a very simple two-step process. Please note that the pin numbers markings on the ADIS1644X/FLEX were incorrect in early manufacturing lots. Please ignore the pin number markings on the ADIS1644X/FLEX and use the following instructions to guide the connection process. |
| |
| |
^ ^ ^ ^ | ^ ^ ^ ^ |
|{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_install_insertion_00.jpg?230|}} |{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_install_insertion_01.jpg?320|}} |{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_install_insertion_02.jpg?300|}}| | |{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_install_insertion_00.jpg?230|}} |{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_install_insertion_01.jpg?320|}} |{{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_install_insertion_02.jpg?300|}}| |
| |
| Here is an example of what this will look like, after finishing these steps: |
| {{:resources:eval:user-guides:inertial-mems:imu:adis16imu2_wiki_functional_00.jpg?600|}} |
| |
| |