Wiki

This version is outdated by a newer approved version.DiffThis version (10 Dec 2016 00:35) is a draft.
Approvals: 0/1

This is an old revision of the document!


ADIS16ACL2/PCB WIKI GUIDE

OVERVIEW

The ADIS16223 and ADIS16227 products use a 14-pin flexible interface. The mating connector for their interface supports surface-mount solder attachment but does not support direct attachment with ribbon cables. For those who are would like to connect the ADIS16223 and ADIS16227 to an existing processor board, using a ribbon cable, the ADIS16ACL2/PCBZ provides a simple connector translation for this purpose.

ORDERING

To order this breakout board, please visit the ADIS16ACL1/PCBZ's web page at TBD…

ADIS16223/ADIS16227 Connection

ADD INSTRUCTION HERE

EVAL-ADIS2 Connection

The EVAL-ADIS2 provides PC-based evaluation support for the ADIS16210 and ADIS16228. J1 on the EVAL-ADIS2Z and the ADIS16ACL1/PCBZ use the same pin assignments, so connecting them requires a 16-pin ribbon cable.

Electrical Schematic

Outer Dimensions

Mounting Holes

resources/eval/user-guides/inertial-mems/imu/adis16acl2-pcb.1481326539.txt.gz · Last modified: 10 Dec 2016 00:35 by Mark Looney