This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:inertial-mems:imu:adis1647x-pcb [12 Apr 2019 19:26] – [ELECTRICAL SCHEMATIC] Mark Looney | resources:eval:user-guides:inertial-mems:imu:adis1647x-pcb [03 Jan 2021 22:04] (current) – fix links Robin Getz | ||
---|---|---|---|
Line 10: | Line 10: | ||
- | =====PART NUMBER SUMMARY===== | + | =====ORDERING GUIDE/ |
Please see the follow table for a list of available breakout boards, along with the IMU model number that is on each board. | Please see the follow table for a list of available breakout boards, along with the IMU model number that is on each board. | ||
^ MODEL NUMBERS | ^ MODEL NUMBERS | ||
^ BREAKOUT BOARD ^ IMU ^ GYROSCOPE ^ ACCELEROMETER ^ | ^ BREAKOUT BOARD ^ IMU ^ GYROSCOPE ^ ACCELEROMETER ^ | ||
- | | ADIS16470/ | + | | [[adi> |
- | | ADIS16475-1/ | + | | [[adi> |
- | | ADIS16475-2/ | + | | [[adi> |
- | | ADIS16475-3/ | + | | [[adi> |
- | | ADIS16477-1/ | + | | [[adi> |
- | | ADIS16477-2/ | + | | [[adi> |
- | | ADIS16477-3/ | + | | [[adi> |
=====EVAL-ADIS2 CONNECTION===== | =====EVAL-ADIS2 CONNECTION===== | ||
Line 32: | Line 32: | ||
These breakout boards, provide four mounting holes, one in each corner, which support attachment to another surface with M2 machine screws. Please see the following diagram for more details: | These breakout boards, provide four mounting holes, one in each corner, which support attachment to another surface with M2 machine screws. Please see the following diagram for more details: | ||
- | {{: | + | {{: |
=====INTERFACE CONNECTOR===== | =====INTERFACE CONNECTOR===== | ||
Please see the following table for the pin assignments for the interface connector (J1) | Please see the following table for the pin assignments for the interface connector (J1) | ||
Line 67: | Line 67: | ||
{{: | {{: | ||
- | =====EMBEDDED | + | =====REFERENCE DESIGNS & CODE EXAMPLES===== |
- | The following | + | For those who are ready to evaluate the ADIS1647x, this section provides a list of reference designs. |
+ | |||
+ | - Physical connection, between the ADIS1647x-x/PCB and a specific | ||
+ | |||
+ | - Embedded | ||
[[https:// | [[https:// |