This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:inertial-mems:imu:adis1647x-pcb [12 Oct 2017 17:42] – [ELECTRICAL SCHEMATIC] Mark Looney | resources:eval:user-guides:inertial-mems:imu:adis1647x-pcb [03 Jan 2021 22:04] (current) – fix links Robin Getz | ||
---|---|---|---|
Line 10: | Line 10: | ||
- | =====PART NUMBER SUMMARY===== | + | =====ORDERING GUIDE/ |
Please see the follow table for a list of available breakout boards, along with the IMU model number that is on each board. | Please see the follow table for a list of available breakout boards, along with the IMU model number that is on each board. | ||
+ | ^ MODEL NUMBERS | ||
+ | ^ BREAKOUT BOARD ^ IMU ^ GYROSCOPE ^ ACCELEROMETER ^ | ||
+ | | [[adi> | ||
+ | | [[adi> | ||
+ | | [[adi> | ||
+ | | [[adi> | ||
+ | | [[adi> | ||
+ | | [[adi> | ||
+ | | [[adi> | ||
- | ^ BREAKOUT BOARD ^ IMU MODEL NUMBER^ | + | =====EVAL-ADIS2 CONNECTION===== |
- | | ADIS16470/ | + | The J1 connector on each ADIS1647x breakout board is pin-for-pin compatible with the same connector (J1) on the [[adi> |
- | | ADIS16475-1/PCBZ | ADIS16475-1BMLZ | | + | |
- | | ADIS16475-2/PCBZ | ADIS16475-2BMLZ | | + | |
- | | ADIS16475-3/ | + | |
- | | ADIS16477-1/ | + | |
- | | ADIS16477-2/ | + | |
- | | ADIS16477-3/ | + | |
+ | **UNDER CONSTRUCTION** | ||
=====DIMENSTIONS/ | =====DIMENSTIONS/ | ||
Line 29: | Line 32: | ||
These breakout boards, provide four mounting holes, one in each corner, which support attachment to another surface with M2 machine screws. Please see the following diagram for more details: | These breakout boards, provide four mounting holes, one in each corner, which support attachment to another surface with M2 machine screws. Please see the following diagram for more details: | ||
- | {{: | + | {{: |
=====INTERFACE CONNECTOR===== | =====INTERFACE CONNECTOR===== | ||
Please see the following table for the pin assignments for the interface connector (J1) | Please see the following table for the pin assignments for the interface connector (J1) | ||
Line 64: | Line 67: | ||
{{: | {{: | ||
+ | =====REFERENCE DESIGNS & CODE EXAMPLES===== | ||
+ | For those who are ready to evaluate the ADIS1647x, this section provides a list of reference designs. | ||
+ | |||
+ | - Physical connection, between the ADIS1647x-x/ | ||
+ | |||
+ | - Embedded code, which lists all ADIS1647x user registers, manages the ADIS1647x' | ||
+ | [[https:// |