Wiki

This version is outdated by a newer approved version.DiffThis version (23 Aug 2017 23:04) is a draft.
Approvals: 0/1

This is an old revision of the document!


ADIS16470/PCBZ BREAKOUT BOARD WIKI GUIDE

OVERVIEW

The ADIS16470/PCBZ is a breakout board that provides a simple way to develop a prototype connection between the ADIS16470 and an existing embedded processor platform. This breakout board already contains one ADIS16470AMLZ and one 16-pin header, which mates to 2 mm ribbon cables. As a general guideline, the ADIS16470/PCBZ supports reliable communications over ribbon cables that are up to 20 cm in length, but it is always a good idea to validate signal integrity before relying on this type of connection to support a critical communication link.

ORDERING

To order this breakout board, please visit

ACTION: REQUEST WEB PAGE FOR ADIS16470/PCB

DIMENSTIONS/MOUNTING HOLES

The ADIS16470/PCBZ provides four mounting holes, one in each corner, which support attachment to another surface with M2 machine screws. Please see the following diagram for more details:

INTERFACE CONNECTOR

Please see the following table for the pin assignments for the interface connector (J1)

PIN NAME DESCRIPTION
1 ~RST Reset, Active Low
2 SCLK Serial Clock (Serial Peripheral Interface)
3 ~CS Chip Select (Serial Peripheral Interface), Active Low
4 DOUT Data Output (Serial Peripheral Interface)
5 DNC Do not connect
6 DIN Data Input (Serial Peripheral Interface)
7 GND Ground
8 GND Ground
9 GND Ground
10 VDD Power Supply, +3.3V
11 VDD Power Supply, +3.3V
12 VDD Power Supply, +3.3V
13 DR Data Ready
14 SYNC Sync Input
15 DNC Do not connect
16 DNC Do not connect

CABLING

J1 supports standard 1mm ribbon cables.

ACTION: write up something about the cable lengths

ELECTRICAL SCHEMATIC

The following diagram illustrates the electrical schematic for the ADIS16470/PCBZ. Click on this image to access a higher-resolution view.

resources/eval/user-guides/inertial-mems/imu/adis1647x-pcb.1503522256.txt.gz · Last modified: 23 Aug 2017 23:04 by Mark Looney