This is an old revision of the document!
The ADIS16470/PCBZ is a breakout board that provides a simple way to develop a prototype connection between the ADIS16470 and an existing embedded processor platform. This breakout board already contains one ADIS16470AMLZ and one 16-pin header, which mates to 2 mm ribbon cables. As a general guideline, the ADIS16470/PCBZ supports reliable communications over ribbon cables that are up to 20 cm in length, but it is always a good idea to validate signal integrity before relying on this type of connection to support a critical communication link.
To order this breakout board, please visit
ACTION: REQUEST WEB PAGE FOR ADIS16470/PCB
The ADIS16470/PCBZ provides four mounting holes, one in each corner, which support attachment to another surface with M2 machine screws. Please see the following diagram for more details:
Please see the following table for the pin assignments for the interface connector (J1)
PIN | NAME | DESCRIPTION |
---|---|---|
1 | ~RST | Reset, Active Low |
2 | SCLK | Serial Clock (Serial Peripheral Interface) |
3 | ~CS | Chip Select (Serial Peripheral Interface), Active Low |
4 | DOUT | Data Output (Serial Peripheral Interface) |
5 | DNC | Do not connect |
6 | DIN | Data Input (Serial Peripheral Interface) |
7 | GND | Ground |
8 | GND | Ground |
9 | GND | Ground |
10 | VDD | Power Supply, +3.3V |
11 | VDD | Power Supply, +3.3V |
12 | VDD | Power Supply, +3.3V |
13 | DR | Data Ready |
14 | SYNC | Sync Input |
15 | DNC | Do not connect |
16 | DNC | Do not connect |
J1 supports standard 1mm ribbon cables.
ACTION: write up something about the cable lengths