This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:inertial-mems:imu:adis1647x-pcb [21 Aug 2019 03:29] – [PART NUMBER SUMMARY] Mark Looney | resources:eval:user-guides:inertial-mems:imu:adis1647x-pcb [24 Aug 2020 21:32] – [DIMENSTIONS/MOUNTING HOLES] Paul Kern | ||
---|---|---|---|
Line 10: | Line 10: | ||
- | =====PART NUMBER SUMMARY===== | + | =====ORDERING GUIDE/ |
Please see the follow table for a list of available breakout boards, along with the IMU model number that is on each board. | Please see the follow table for a list of available breakout boards, along with the IMU model number that is on each board. | ||
Line 32: | Line 32: | ||
These breakout boards, provide four mounting holes, one in each corner, which support attachment to another surface with M2 machine screws. Please see the following diagram for more details: | These breakout boards, provide four mounting holes, one in each corner, which support attachment to another surface with M2 machine screws. Please see the following diagram for more details: | ||
- | {{: | + | {{: |
=====INTERFACE CONNECTOR===== | =====INTERFACE CONNECTOR===== | ||
Please see the following table for the pin assignments for the interface connector (J1) | Please see the following table for the pin assignments for the interface connector (J1) |