Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:inertial-mems:imu:adis16227-adisusb [08 Oct 2013 03:41] – [USB Driver Installation] Mark Looneyresources:eval:user-guides:inertial-mems:imu:adis16227-adisusb [27 Jan 2021 22:34] (current) – use wp> interwiki links Robin Getz
Line 137: Line 137:
 {{:resources:eval:user-guides:inertial-mems:imu:adisusb-driver-complete-wizard.png?400|}} {{:resources:eval:user-guides:inertial-mems:imu:adisusb-driver-complete-wizard.png?400|}}
  
-<wrap alert> **WARNING:** For those who are using Windows XP, Service Pack 3, additional steps are required for completing the driver installation.  Please see page 8, on the **[[http://www.analog.com/static/imported-files/user_guides/UG-363.pdf#Page=08|ADISUSB User Guide (UG-363)]]** for additional information on these steps. </wrap>+<wrap alert> **WARNING:** For those who are using Windows XP, Service Pack 3, additional steps are required for completing the driver installation.  Please see page 8, on the **[[adi>static/imported-files/user_guides/UG-363.pdf#Page=08|ADISUSB User Guide (UG-363)]]** for additional information on these steps. </wrap>
 ===== ADIS16227 Evaluation SOFTWARE  ===== ===== ADIS16227 Evaluation SOFTWARE  =====
 After the USB driver installation is complete, connect the [[adi>ADISUSB|ADISUSB]] USB connector to the PC, using the USB Mini cable, from the [[adi>ADISUSB|ADISUSB]] kit. D2 will illuminate as soon as this connection is made. This indicates that the [[adi>ADISUSB|ADISUSB]] has power and is going through its start-up/initialization process. During the initialization process, several messages may appear on the screen. They are related to updating the [[adi>ADISUSB|ADISUSB]] firmware and establishing communication between the PC and the [[adi>ADISUSB|ADISUSB]]. After the updates are finished double click on the ADiS16227_Eval_Rev_2.exe file to launch the software application. After the USB driver installation is complete, connect the [[adi>ADISUSB|ADISUSB]] USB connector to the PC, using the USB Mini cable, from the [[adi>ADISUSB|ADISUSB]] kit. D2 will illuminate as soon as this connection is made. This indicates that the [[adi>ADISUSB|ADISUSB]] has power and is going through its start-up/initialization process. During the initialization process, several messages may appear on the screen. They are related to updating the [[adi>ADISUSB|ADISUSB]] firmware and establishing communication between the PC and the [[adi>ADISUSB|ADISUSB]]. After the updates are finished double click on the ADiS16227_Eval_Rev_2.exe file to launch the software application.
Line 198: Line 198:
  
 The green box identifies the configuration box for the name and location of the data storage file. The green box identifies the configuration box for the name and location of the data storage file.
-The yellow box identifies a number of configuration options for the data acquisition process. The **Scaled Units** option causes the software to convert the decimal, twos complement number into its representative value.  For example, when enabling **Use Scaled Data,** the accelerometer outputs will  be in units of g's [[http://en.wikipedia.org/wiki/G-force|g-force]].+The yellow box identifies a number of configuration options for the data acquisition process. The **Scaled Units** option causes the software to convert the decimal, twos complement number into its representative value.  For example, when enabling **Use Scaled Data,** the accelerometer outputs will  be in units of g's [[wp>G-force|g-force]].
  
 ==== EXAMPLE EXERCISES ==== ==== EXAMPLE EXERCISES ====
 This section currently has no [[adi>ADIS16227|ADIS16227]]-specific content, but the This section currently has no [[adi>ADIS16227|ADIS16227]]-specific content, but the
-[[http://wiki.analog.com/resources/eval/user-guides/inertial-mems/imu/adis16448?&#example_evaluation_exercises|ADIS16448 Evaluation on the EVAL-ADIS Wiki Site]] has some good examples to start with.+[[/resources/eval/user-guides/inertial-mems/imu/adis16448?&#example_evaluation_exercises|ADIS16448 Evaluation on the EVAL-ADIS Wiki Site]] has some good examples to start with.
resources/eval/user-guides/inertial-mems/imu/adis16227-adisusb.1381196465.txt.gz · Last modified: 08 Oct 2013 03:41 by Mark Looney