Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
Last revisionBoth sides next revision
resources:eval:user-guides:inertial-mems:imu:adis16223-adisusb [19 Nov 2012 16:26] – [Data Capture Menu] Scott Hutchensresources:eval:user-guides:inertial-mems:imu:adis16223-adisusb [28 Aug 2014 23:14] – [Example Exercises] Mark Looney
Line 78: Line 78:
 {{:resources:eval:user-guides:inertial-mems:imu:223-pcbz-schematic.png?400|}} {{:resources:eval:user-guides:inertial-mems:imu:223-pcbz-schematic.png?400|}}
    
-NOTE: Do not plug the [[adi>ADISUSB|ADISUSB]] into the USB cable at this stage of the setup.  Wait until the software installation is complete.+<WRAP center round important 60%> 
 +Do not plug the [[adi>ADISUSB|ADISUSB]] into the USB cable at this stage of the setup.  Wait until the software installation is complete. 
 +</WRAP> 
 + 
  
 === Step #1 === === Step #1 ===
Line 86: Line 90:
 {{:resources:eval:user-guides:inertial-mems:imu:223-pcbz-part-mounted.png?400|}} {{:resources:eval:user-guides:inertial-mems:imu:223-pcbz-part-mounted.png?400|}}
  
-WARNING: Make sure that the connector cable going from J1 on the [[adi>en/mems-sensors/mems-accelerometers/adis16223/products/EVAL-ADIS16223/eb.html|ADIS16223/PCBZ]] is properly aligned to the J1 connector on the [[adi>ADISUSB|ADISUSB]]. The 12 pin cable is included with the [[adi>ADISUSB|ADISUSB]].+<WRAP center round alert 60%> 
 +Make sure that the connector cable going from J1 on the [[adi>en/mems-sensors/mems-accelerometers/adis16223/products/EVAL-ADIS16223/eb.html|ADIS16223/PCBZ]] is properly aligned to the J1 connector on the [[adi>ADISUSB|ADISUSB]]. The 12 pin cable is included with the [[adi>ADISUSB|ADISUSB]]. 
 +</WRAP> 
  
 === Step #2 === === Step #2 ===
Line 184: Line 191:
 {{:resources:eval:user-guides:inertial-mems:imu:223-datalog-defined.png?400|}} {{:resources:eval:user-guides:inertial-mems:imu:223-datalog-defined.png?400|}}
  
-**Note:** The Main screen datalog option should be checked to enable the datalog function.+<WRAP center round alert 60%> 
 +The Main screen datalog option should be checked to enable the datalog function. 
 +</WRAP> 
 + 
  
 The green box identifies the configuration box for the name and location of the data storage file. The green box identifies the configuration box for the name and location of the data storage file.
Line 190: Line 201:
 The yellow box identifies a number of configuration options for the data acquisition process. The **Scaled Units** option causes the software to convert the decimal, twos complement number into its representative value.  For example, when enabling **Use Scaled Data,** the accelerometer outputs will  be in units of g's [[http://en.wikipedia.org/wiki/G-force|g-force]]. The yellow box identifies a number of configuration options for the data acquisition process. The **Scaled Units** option causes the software to convert the decimal, twos complement number into its representative value.  For example, when enabling **Use Scaled Data,** the accelerometer outputs will  be in units of g's [[http://en.wikipedia.org/wiki/G-force|g-force]].
  
-==== EXAMPLE EXERCISES ==== + 
-This section currently has no [[adi>ADIS16223|ADIS16223]]-specific content, but the + 
-[[http://wiki.analog.com/resources/eval/user-guides/inertial-mems/imu/adis16448?&#example_evaluation_exercises|ADIS16448 Evaluation on the EVAL-ADIS Wiki Site]] has some good examples to start with.+==== Example Exercises ==== 
 + 
 +**Demonstrating the Averaging/Decimation Function** 
 + 
 +Screen shots of  the 16220_Eval_Rev_5 software running an [[adi>ADIS16223|ADIS16223]] device. 
 +In each graphic the value of the AVG_CNT increases from 1 to 1024. 
 +Notice that the Capture Duration also increases from 0.23 seconds to 16.90 seconds. 
 +Plots show that the data noise is reduced as the AVG_CNT is increased. This gives the customer greater flexibility for their specific application. 
 + 
 +<WRAP center round tip 60%> 
 +When the [[adi>ADIS16223|ADIS16223]] Capture Mode is set to Periodic then the CAP_PRD must be set by the user to a value greater than the Capture Duration. 
 +</WRAP> 
 + 
 +{{:resources:eval:user-guides:inertial-mems:imu:223-avg-deci-1.png?400 |}} 
 +{{:resources:eval:user-guides:inertial-mems:imu:223-avg-deci-2.png?400 |}} 
 +{{:resources:eval:user-guides:inertial-mems:imu:223-avg-deci-4.png?400 |}} 
 +{{:resources:eval:user-guides:inertial-mems:imu:223-avg-deci-8.png?400 |}} 
 +{{:resources:eval:user-guides:inertial-mems:imu:223-avg-deci-16.png?400 |}} 
 +{{:resources:eval:user-guides:inertial-mems:imu:223-avg-deci-32.png?400 |}} 
 +{{:resources:eval:user-guides:inertial-mems:imu:223-avg-deci-64.png?400 |}} 
 +{{:resources:eval:user-guides:inertial-mems:imu:223-avg-deci-128.png?400 |}} 
 +{{:resources:eval:user-guides:inertial-mems:imu:223-avg-deci-256.png?400 |}} 
 +{{:resources:eval:user-guides:inertial-mems:imu:223-avg-deci-512.png?400 |}} 
 +{{:resources:eval:user-guides:inertial-mems:imu:223-avg-deci-1024.png?400|}} 
 + 
 +<WRAP center round box 60%> 
 +</WRAP> 
 + 
  
resources/eval/user-guides/inertial-mems/imu/adis16223-adisusb.txt · Last modified: 27 Jan 2021 22:34 by Robin Getz