This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:inertial-mems:imu:adis16210-pcb [06 Jul 2016 20:43] – [INTERFACE PCB] Mark Looney | resources:eval:user-guides:inertial-mems:imu:adis16210-pcb [07 Jul 2016 04:26] (current) – [ELECTRICAL SCHEMATIC] Mark Looney | ||
---|---|---|---|
Line 8: | Line 8: | ||
=====INTERFACE PCB===== | =====INTERFACE PCB===== | ||
The interface PCB provides access to the ADIS16210CMLZ, | The interface PCB provides access to the ADIS16210CMLZ, | ||
- | ====ELECTRICAL SCHEMATIC==== | + | ====Mechanical Drawing==== |
- | Insert schematic here | + | |
- | ====INTERFACE CONNECTOR==== | + | {{: |
- | J1 is the electrical connector that provides direct access to power, ground and critical digital I/O pins on the devices. It is a 16-pin, dual-row, 2-mm pitch connector that support 1mm ribbon cable systems. | + | |
- | ===Pin Assignments=== | + | ====Electrical Schematic==== |
+ | Please see the following graphic for the Interface PCB's electrical schematic: | ||
- | Here is the pin assignments for J1, which is the connector that will interface with an embedded processor board. | + | {{: |
+ | ====INTERFACE CONNECTOR PIN ASSIGNMENTS==== | ||
+ | J1 is the electrical connector that provides direct access to power, ground and critical digital I/O pins on the devices. It is a 16-pin, dual-row, 2-mm pitch connector that support 1mm ribbon cable systems. Here is the pin assignments for J1: | ||
{{: | {{: | ||
- | ===Ribbon Cable Options=== | + | NOTE: The ADIS16210CMLZ does not support DIO3 and DIO4, so pins 15 and 16 are not connected. |
- | Check out the following link for ideas on how to make or purchase 16-pin, 1mm ribbon cables that can mate to the ADIS16IMU2/PCBZ. | + | |
- | ====PHYSICAL SETUP==== | + | Check out the following link for ideas on how to make or purchase 16-pin, 1mm ribbon cables that can mate to the ADIS16210/PCBZ. |
+ | |||
+ | [[ez> | ||
+ | =====PHYSICAL SETUP===== | ||
Installing the ADIS16210CMLZ onto the Interface board requires two steps: | Installing the ADIS16210CMLZ onto the Interface board requires two steps: | ||
1. Insert the end of the flex cable (ADIS16210CMLZ) into J2 on the interface board. Check out the video attachment at this link for a demonstration. | 1. Insert the end of the flex cable (ADIS16210CMLZ) into J2 on the interface board. Check out the video attachment at this link for a demonstration. | ||
+ | |||
+ | [[ez> | ||
2. Secure the ADIS16210CMLZ base to the Interface PCB, using four M2x0.4mm machine screws | 2. Secure the ADIS16210CMLZ base to the Interface PCB, using four M2x0.4mm machine screws | ||
- | ====INTERFACE CONNECTOR==== | + | 3. Connect |
- | J1 is the electrical connector that provides direct access to power, ground and critical digital I/O pins on the devices. It is a 16-pin, dual-row, 2-mm pitch connector that support 1mm ribbon cable systems. | + | |
- | ===Pin Assignments=== | + | =====USE WITH THE EVAL-ADIS SYSTEM===== |
+ | Click on the following link to access instructions for using the ADIS16210/ | ||
- | Here is the pin assignments for J1, which is the connector that will interface with an embedded processor board. | + | [[adis16210|ADIS16210 Evaluation on a PC]] |
- | {{: | ||
- | ===Ribbon Cable Options=== | ||
- | Check out the following link for ideas on how to make or purchase 16-pin, 1mm ribbon cables that can mate to the ADIS16IMU2/ |