Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
resources:eval:user-guides:inertial-mems:imu:adis16209 [27 Jun 2016 19:02] – [Step #1] Mark Looney | resources:eval:user-guides:inertial-mems:imu:adis16209 [27 Jun 2016 19:32] – [Step #1] Mark Looney |
---|
**NOTE:** Do not plug the [[adi>EVAL-ADIS|EVAL-ADIS]] into the USB cable at this stage of the setup. Wait until the software installation is complete. | **NOTE:** Do not plug the [[adi>EVAL-ADIS|EVAL-ADIS]] into the USB cable at this stage of the setup. Wait until the software installation is complete. |
</WRAP> | </WRAP> |
| } |
====Step #1==== | ====Step #1==== |
Connect the [[adi>EVAL-ADIS16209|ADIS16209/PCBZ]] to the [[adi>EVAL-ADIS|EVAL-ADIS]], using the ribbon cable (comes with [[adi>EVAL-ADIS|EVAL-ADIS]]) and **J1** on both boards. **J1** on both boards share common pin assignments, for pins 1 through 12. So, make sure that the ribbon cable connects pins 1-12 on both **J1** connectors. Since the [[adi>EVAL-ADIS16209|ADIS16209/PCBZ]] (J1) has only 12 pins, pins 13, 14, 15 and 16 on the [[adi>EVAL-ADIS|EVAL-ADIS]] (J1) will remain unconnected through the ribbon cable. | Connect the [[adi>EVAL-ADIS16209|ADIS16209/PCBZ]] to the [[adi>EVAL-ADIS|EVAL-ADIS]], using the ribbon cable (comes with [[adi>EVAL-ADIS|EVAL-ADIS]]) and **J1** on both boards. **J1** on both boards share common pin assignments, for pins 1 through 12. So, make sure that the ribbon cable connects pins 1-12 on both **J1** connectors. |
| |
| {{:resources:eval:user-guides:inertial-mems:imu:adis16209_pc_eval_wikiguide_01a.png?600|}} |
| |
| Since the [[adi>EVAL-ADIS16209|ADIS16209/PCBZ]] (J1) has only 12 pins, pins 13, 14, 15 and 16 on the [[adi>EVAL-ADIS|EVAL-ADIS]] (J1) will remain unconnected through the ribbon cable. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:209pcbz.png?400|}} | {{:resources:eval:user-guides:inertial-mems:imu:adis16209_pc_eval_wikiguide_01.png?600|}} |
| |
====Step #2==== | ====Step #2==== |