This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:inertial-mems:imu-overview [21 Jul 2021 01:21] – [Vibration Rectification Error (VRE)] Chas Frick | resources:eval:user-guides:inertial-mems:imu-overview [31 Aug 2021 22:00] (current) – [Linear Acceleration Effect (Linear-g), Linear Acceleration Effect on Bias, Linear-g Rejection (Linear-g Sensitivity)] Chas Frick | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== ADI MEMS IMUs Glossary: Performance Characteristics, | ====== ADI MEMS IMUs Glossary: Performance Characteristics, | ||
This page is intended to introduce and discuss common characteristics of MEMS IMUs, how to measure those performance metrics and finally some applications where those metrics matter. | This page is intended to introduce and discuss common characteristics of MEMS IMUs, how to measure those performance metrics and finally some applications where those metrics matter. | ||
+ | |||
+ | ====== Bias Repeatability ====== | ||
+ | Measured in °/hour. | ||
====== Bias Error ====== | ====== Bias Error ====== | ||
- | Offset error in MEMs output on a particular axis. Fixed error typically. | + | Offset error in MEMs output on a particular axis. Fixed error typically. Measured in °/hour. |
====== Sensitivity Error ====== | ====== Sensitivity Error ====== | ||
Line 14: | Line 17: | ||
This can be thought of as the sensor resolution in an "ideal case." It is also found as the minimum of the AVAR plot. | This can be thought of as the sensor resolution in an "ideal case." It is also found as the minimum of the AVAR plot. | ||
- | ====== | + | ====== |
- | Applies to gyroscopes. It is the " | + | Measured |
- | ====== | + | Applies to gyroscopes. It is the " |
+ | |||
+ | For an example consider the ADIS16153, with datasheet here: [[adi> | ||
+ | {{ : | ||
+ | |||
+ | |||
+ | |||
+ | |||
+ | Additional notes: [[http:// | ||
+ | |||
+ | |||
+ | ====== Rate Random Walk (ARRW) ====== | ||
Applies to gyroscopes and is the "far out" (large Τ) on the Allan Variance (AVAR) curve. | Applies to gyroscopes and is the "far out" (large Τ) on the Allan Variance (AVAR) curve. | ||
This quantity represents long-term stability of the sensor measurement. | This quantity represents long-term stability of the sensor measurement. | ||
Line 29: | Line 43: | ||
Can be approximated with the formula: ND ≅ ARW/60* √2 | Can be approximated with the formula: ND ≅ ARW/60* √2 | ||
- | ====== Linear Acceleration Effect (Linear-g) ====== | ||
- | Measured in degrees/ | ||
====== Vibration Rectification Error (VRE) ====== | ====== Vibration Rectification Error (VRE) ====== | ||
Line 36: | Line 48: | ||
====== Cross-Axis Sensitivity ====== | ====== Cross-Axis Sensitivity ====== | ||
- | Unintended effect where rotation/ | + | Unintended effect where rotation/ |
+ | Can be calculated from axis to axis misalignment error for accels/ | ||
+ | |||
+ | Example: For the ADIS16448, the accel axis to axis misalignment is 0.2 degrees. Therefore Cross-axis sensitivity accel is sin(0.2) = 0.197%. Gyro is sin(0.05) = 0.09%. Magnetometer: | ||
+ | |||
+ | ====== Linear Acceleration Effect (Linear-g), Linear Acceleration Effect on Bias, Linear-g Rejection (Linear-g Sensitivity) ====== | ||
+ | Unintended effect where linear acceleration is detected as rotation. Measured in degrees/ | ||
+ | |||
+ | ====== Vibration Rejection (Gyros) ====== | ||
+ | A combination of Linear-g and Vibration Rectification (VRE) specs. | ||
+ | |||
+ | Vibration response of a gyro = Linear-g X-Axis Acceleration + (VRE X-Axis Acceleration)^2 | ||
- | ====== | + | ====== |
- | Unintended effect where linear acceleration is detected as rotation | + | * Information on Allan Variance for Gyros: http:// |