Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision |
resources:eval:user-guides:inertial-mems:gyroscopes:adis1626x-adisusb [08 Oct 2013 03:42] – [USB Driver Installation] Mark Looney | resources:eval:user-guides:inertial-mems:gyroscopes:adis1626x-adisusb [03 Jan 2021 22:04] – fix links Robin Getz |
---|
{{:resources:eval:user-guides:inertial-mems:imu:adisusb-driver-complete-wizard.png?400|}} | {{:resources:eval:user-guides:inertial-mems:imu:adisusb-driver-complete-wizard.png?400|}} |
| |
<wrap alert> **WARNING:** For those who are using Windows XP, Service Pack 3, additional steps are required for completing the driver installation. Please see page 8, on the **[[http://www.analog.com/static/imported-files/user_guides/UG-363.pdf#Page=08|ADISUSB User Guide (UG-363)]]** for additional information on these steps. </wrap> | <wrap alert> **WARNING:** For those who are using Windows XP, Service Pack 3, additional steps are required for completing the driver installation. Please see page 8, on the **[[adi>static/imported-files/user_guides/UG-363.pdf#Page=08|ADISUSB User Guide (UG-363)]]** for additional information on these steps. </wrap> |
===== Analog Devices ADIS16260/5 Evaluation SOFTWARE ===== | ===== Analog Devices ADIS16260/5 Evaluation SOFTWARE ===== |
After the USB driver installation is complete, connect the [[adi>ADISUSB|ADISUSB]] USB connector to the PC, using the USB Mini cable, from the [[adi>ADISUSB|ADISUSB]] kit. D2 will illuminate as soon as this connection is made. This indicates that the [[adi>ADISUSB|ADISUSB]] has power and is going through its start-up/initialization process. During the initialization process, several messages may appear on the screen. They are related to updating the [[adi>ADISUSB|ADISUSB]] firmware and establishing communication between the PC and the [[adi>ADISUSB|ADISUSB]]. After the updates are finished double click on the setup.exe file to launch the software application. | After the USB driver installation is complete, connect the [[adi>ADISUSB|ADISUSB]] USB connector to the PC, using the USB Mini cable, from the [[adi>ADISUSB|ADISUSB]] kit. D2 will illuminate as soon as this connection is made. This indicates that the [[adi>ADISUSB|ADISUSB]] has power and is going through its start-up/initialization process. During the initialization process, several messages may appear on the screen. They are related to updating the [[adi>ADISUSB|ADISUSB]] firmware and establishing communication between the PC and the [[adi>ADISUSB|ADISUSB]]. After the updates are finished double click on the setup.exe file to launch the software application. |