Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:inertial-mems:gyroscopes:adis16265-eval-adis [04 Sep 2013 15:25] – [OVERVIEW] Scott Hutchens | resources:eval:user-guides:inertial-mems:gyroscopes:adis16265-eval-adis [09 Oct 2013 03:30] (current) – [Main Window] Mark Looney |
---|
| |
===== PHYSICAL SETUP ===== | ===== PHYSICAL SETUP ===== |
The [[adi>ADIS16209|EVAL-ADIS16209]] provides the [[adi>ADIS16209|EVAL-ADIS16209]] function on a 1.2 inch × 1.3 inch printed circuit board (PCB), which simplifies the connection to an existing processor system. The four mounting holes accommodate either M2 (2mm) or Type 2-56 machine screws. These boards are made of IS410 | The [[adi>ADIS16265|ADIS16265]] provides the [[adi>ADIS16265|EVAL-ADIS16265]] function on a 1.2 inch × 1.3 inch printed circuit board (PCB), which simplifies the connection to an existing processor system. The four mounting holes accommodate either M2 (2mm) or Type 2-56 machine screws. These boards are made of IS410 |
material and are 0.063 inches thick. The second level assembly uses a SAC305-compatible solder composition (Pb-free), which has a pre-solder re-flow thickness of approximately 0.005 inches. The pad pattern on the [[adi>EVAL-ADIS16209|ADIS16209/PCBZ]] matches that shown in below. J1 and J2 are dual-row, 2 mm (pitch) connectors that work with a number of ribbon cable systems, including 3M Part Number 152212-0100-GB (ribbon-crimp connector) and 3M Part Number 3625/12 (ribbon cable). | material and are 0.063 inches thick. The second level assembly uses a SAC305-compatible solder composition (Pb-free), which has a pre-solder re-flow thickness of approximately 0.005 inches. The pad pattern on the [[adi>EVAL-ADIS16265|ADIS16265/PCBZ]] matches that shown in below. J1 and J2 are dual-row, 2 mm (pitch) connectors that work with a number of ribbon cable systems, including 3M Part Number 152212-0100-GB (ribbon-crimp connector) and 3M Part Number 3625/12 (ribbon cable). |
| |
{{:resources:eval:user-guides:inertial-mems:imu:220-pcbz-dimensions.png?300 |}} | {{:resources:eval:user-guides:inertial-mems:imu:220-pcbz-dimensions.png?300 |}} |
| |
=== Step #1 === | === Step #1 === |
The connection to the [[adi>EVAL-ADIS16209|ADIS16209/PCBZ]] is simple using J1 and a 16 pin cable included with the [[adi>EVAL-ADIS|EVAL-ADIS]]. | The connection to the [[adi>EVAL-ADIS16265|ADIS16265/PCBZ]] is simple using J1 and a 16 pin cable included with the [[adi>EVAL-ADIS|EVAL-ADIS]]. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:209pcbz.png?400|}} | {{ :resources:eval:user-guides:inertial-mems:gyroscopes:265pcbz.png?600 |}} |
| |
<WRAP center round alert 60%> | <WRAP center round alert 80%> |
**WARNING:** | **WARNING:** |
Make sure that the connector cable going from J1 on the [[adi>EVAL-ADIS16209|ADIS16209/PCBZ]] is properly aligned to the J1 connector on the [[adi>EVAL-ADIS|EVAL-ADIS]]. The 16 pin cable is included with the [[adi>EVAL-ADIS|EVAL-ADIS]] and proper mating has the last 4 cable connections open. The yellow wire from from J2-11 of the [[adi>EVAL-ADIS16209|ADIS16209/PCBZ]] to the DIO1 test point on the [[adi>EVAL-ADIS|EVAL-ADIS]] is only required for synchronous data.</WRAP> | Make sure that the connector cable going from J1 on the [[adi>EVAL-ADIS16265|ADIS16265/PCBZ]] is properly aligned to the J1 connector on the [[adi>EVAL-ADIS|EVAL-ADIS]]. The 16 pin cable is included with the [[adi>EVAL-ADIS|EVAL-ADIS]] and proper mating has the last 4 cable connections open. The Black wire from from J2-12 of the [[adi>EVAL-ADIS16265|ADIS16265/PCBZ]] to the DIO1 test point on the [[adi>EVAL-ADIS|EVAL-ADIS]] is only required for synchronous data.</WRAP> |
| |
{{:resources:eval:user-guides:inertial-mems:imu:209-cable-conn.png?400 |}} | {{:resources:eval:user-guides:inertial-mems:gyroscopes:265mnt-on-eval-adis-j1conn.png?420|}} |
{{:resources:eval:user-guides:inertial-mems:imu:209-data-ready-wire.png?400 |}} | {{:resources:eval:user-guides:inertial-mems:gyroscopes:265eval-adis-data-ready.png?400|}} |
| |
=== Step #2 === | === Step #2 === |
Mounting to the system frame is accomplished using 4 M2x.4x4mm machine screws included with the [[adi>EVAL-ADIS16209|ADIS16209/PCBZ]]. The mounting location holes are marked as an example in the picture below. Use the 4 A-location holes to secure the [[adi>EVAL-ADIS16209|ADIS16209/PCBZ]] to the [[adi>EVAL-ADIS|EVAL-ADIS]]. | Mounting to the system frame is accomplished using 4 M2x.4x4mm machine screws included with the [[adi>EVAL-ADIS16265|ADIS16265/PCBZ]]. The mounting location holes are marked as an example in the picture below. Use the 4 A-location holes to secure the [[adi>EVAL-ADIS16265|ADIS16265/PCBZ]] to the [[adi>EVAL-ADIS|EVAL-ADIS]]. |
| |
{{:resources:eval:user-guides:inertial-mems:imu:209-eval-locate-holes.png?400 |}} | {{:resources:eval:user-guides:inertial-mems:gyroscopes:265mnt-holes-on-eval-adis.png?350|}} |
{{:resources:eval:user-guides:inertial-mems:imu:209pcbz-eval-adis.png?400|}} | {{:resources:eval:user-guides:inertial-mems:gyroscopes:265-eval-adis-data-rdy.png?500|}} |
| |
=== Step #3 === | === Step #3 === |
The following picture (left side) shows JP1 in the **+3.3V** position (factory-default). That is the correct JP1 jumper setting on the [[adi>EVAL-ADIS|EVAL-ADIS]]) required for the [[adi>EVAL-ADIS16209|ADIS16209CCCZ]]. | The following picture (left side) shows JP1 in the **+3.3V** position (factory-default). That is not the correct JP1 jumper setting on the [[adi>EVAL-ADIS|EVAL-ADIS]]) required for the [[adi>EVAL-ADIS16265|ADIS16265CCCZ]]and should be moved to the ***+5V*** position (right side). |
| |
{{:resources:eval:user-guides:inertial-mems:imu:eval-adis-3.3v.png?400|}} | {{:resources:eval:user-guides:inertial-mems:imu:eval-adis-3.3v.png?350|}} |
| {{:resources:eval:user-guides:inertial-mems:gyroscopes:eval-adis-5v-setting.png?500|}} |
| |
<WRAP center round box 60%> | <WRAP center round box 60%> |
**NOTE:** If JP1 is left on **+5v** the software will look like the following picture. Move JP1 to the**+3.3V** setting to correct the problem. | **NOTE:** If JP1 is left on **+3.3v** position the software will look like the following picture. Move JP1 to the**+5V** setting to correct the problem. |
</WRAP> | </WRAP> |
| |
====IMU EVALUATION SOFTWARE DOWNLOAD/GETTING STARTED==== | {{:resources:eval:user-guides:inertial-mems:gyroscopes:265-main-low-voltage.png?600|}} |
| ====IMU EVALUATION SOFTWARE OVERVIEW==== |
| |
Visit the [[http://wiki.analog.com/resources/eval/user-guides/inertial-mems/imu/imu-evaluation-software|IMU Evaluation Software Wiki Guide]] for software download, driver installation and basic, "getting started" instructions. | {{page> resources/eval/user-guides/inertial-mems/imu/imu-evaluation-software#imu_evaluation_software_overview&nofooter&noheader}} |
| |
QUICK TIP: Right click on this link and open this guide in a new Tab or Window, while keeping this Wiki Guide open. | ====USB Driver Installation==== |
| |
====IMU EVALUATION SOFTWARE FOR THE ADIS16265==== | {{page> resources/eval/user-guides/inertial-mems/imu/imu-evaluation-software#usb_driver_installation&nofooter&noheader}} |
| |
| ====IMU EVALUATION SOFTWARE GETTING STARTED==== |
| |
| {{page> resources/eval/user-guides/inertial-mems/imu/imu-evaluation-software#imu_evaluation_software_starting_point&nofooter&noheader}} |
| |
| |
| ====IMU EVALUATION SOFTWARE REVISION HISTORY==== |
| |
| {{page> resources/eval/user-guides/inertial-mems/imu/imu-evaluation-software#software_revision_history&nofooter&noheader}} |
| |
| |
| |
| |
| |
| |
| APPLICATION TIP: The **Register Access** screen writes to user control registers, inside of the [[adi>ADIS16265|ADIS16265]], two bytes at a time. So, when configuring a register, make sure to include the hexadecimal number for all 16-bits, before pressing the **Write Register** button. When using an embedded processor to write to user control registers, inside of the [[adi>ADIS16265|ADIS16265]], each command (16-bits) writes to one byte at a time. |
| |
| |
| |
| |
| |
| ==== EXAMPLE EXERCISES ==== |
| This section currently has no [[adi>ADIS16265|ADIS16265]]-specific content, but the |
| [[adi>resources/eval/user-guides/inertial-mems/imu/adis16448?&#example_evaluation_exercises|ADIS16448 Evaluation on the EVAL-ADIS Wiki Site]] has some good examples to start with. |
| |