Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:user-guides:inertial-mems:gyroscopes:adis1613x-adisusb [08 Jan 2021 09:43] – Fixed bad link for ADIS16136 Ioana Chelaruresources:eval:user-guides:inertial-mems:gyroscopes:adis1613x-adisusb [09 Jan 2021 00:39] (current) – user interwiki links Robin Getz
Line 27: Line 27:
 {{:resources:eval:user-guides:inertial-mems:imu:adisusb-driver-complete-wizard.png?400|}} {{:resources:eval:user-guides:inertial-mems:imu:adisusb-driver-complete-wizard.png?400|}}
  
-<note important>For those who are using Windows XP, Service Pack 3, additional steps are required for completing the driver installation.  Please see page 8, on the **[[http://www.analog.com/static/imported-files/user_guides/UG-363.pdf#Page=08|ADISUSB User Guide (UG-363)]]** for additional information on these steps.</note>+<note important>For those who are using Windows XP, Service Pack 3, additional steps are required for completing the driver installation.  Please see page 8, on the **[[adi>static/imported-files/user_guides/UG-363.pdf#Page=08|ADISUSB User Guide (UG-363)]]** for additional information on these steps.</note>
  
 After the USB driver installation is complete, connect the [[adi>ADISUSB|ADISUSB]] USB connector to the PC, using the USB Mini cable, from the [[adi>ADISUSB|ADISUSB]] kit. D2 will illuminate as soon as this connection is made. This indicates that the [[adi>ADISUSB|ADISUSB]] has power and is going through its start-up/initialization process. During the initialization process, several messages may appear on the screen. They are related to updating the [[adi>ADISUSB|ADISUSB]] firmware and establishing communication between the PC and the [[adi>ADISUSB|ADISUSB]]. After the updates are finished double click on the setup.exe file to launch the software application. After the USB driver installation is complete, connect the [[adi>ADISUSB|ADISUSB]] USB connector to the PC, using the USB Mini cable, from the [[adi>ADISUSB|ADISUSB]] kit. D2 will illuminate as soon as this connection is made. This indicates that the [[adi>ADISUSB|ADISUSB]] has power and is going through its start-up/initialization process. During the initialization process, several messages may appear on the screen. They are related to updating the [[adi>ADISUSB|ADISUSB]] firmware and establishing communication between the PC and the [[adi>ADISUSB|ADISUSB]]. After the updates are finished double click on the setup.exe file to launch the software application.
resources/eval/user-guides/inertial-mems/gyroscopes/adis1613x-adisusb.1610095427.txt.gz · Last modified: 08 Jan 2021 09:43 by Ioana Chelaru