Wiki

This version is outdated by a newer approved version.DiffThis version (17 Feb 2021 01:52) is a draft.
Approvals: 0/1
The Previously approved version (14 Jan 2021 05:24) is available.Diff

This is an old revision of the document!


EVAL-ADIS2 Evaluation System

The EVAL-ADIS2 has been superceded by the EVAL-ADIS-FX3 and is no longer supported.

The EVAL-ADIS2 is a PC-based evaluation system that supports communication with most ADIS16xxx products, using the “breakout board” evaluation tools for each product. The following diagram illustrates the data sensor data flow when using the EVAL-ADIS2.

The following image identifies the key features associated with this evaluation system.

EVAL-ADIS2 Compatibility Matrix

Expand the table below to view a list of compatible devices, breakout boards, and jumper settings.

Click to display ⇲

Click to hide ⇱

MODEL NUMBER BREAKOUT BOARD JP1 SUPPLY SETTING SOFTWARE PACKAGE
ADIS16133BMLZ ADIS16IMU1/PCBZ +5V IMU Evaluation Software
ADIS16135BMLZ ADIS16IMU1/PCBZ +5V IMU Evaluation Software
ADIS16136BMLZ ADIS16IMU1/PCBZ +5V IMU Evaluation Software
ADIS16137BMLZ ADIS16IMU1/PCBZ +5V IMU Evaluation Software
ADIS16201CCCZ ADIS16201/PCBZ +3.3V IMU Evaluation Software
ADIS16203CCCZ ADIS16203/PCBZ +3.3V IMU Evaluation Software
ADIS16209CCCZ ADIS16209/PCBZ +3.3V IMU Evaluation Software
ADIS16210BMLZ ADIS16ACL1/PCBZ +3.3V IMU Evaluation Software
ADIS16223CMLZ ADIS16ACL2/PCBZ +3.3V ADIS16223 Vibration Evaluation Program
ADIS16227CMLZ ADIS16ACL2/PCBZ +3.3V Vibration Evaluation Program
ADIS16228BMLZ ADIS16ACL1/PCBZ +3.3V Vibration Evaluation Program
ADIS16265BCCZ ADIS16265/PCBZ +5V IMU Evaluation Software
ADIS16334BMLZ ADIS16IMU2/PCBZ and ADIS1644X/FLEX +5V IMU Evaluation Software
ADIS16362BMLZ ADIS16IMU2/PCBZ +5V IMU Evaluation Software
ADIS16364BMLZ ADIS16IMU2/PCBZ +5V IMU Evaluation Software
ADIS16365BMLZ ADIS16IMU2/PCBZ +5V IMU Evaluation Software
ADIS16367BMLZ ADIS16IMU2/PCBZ +5V IMU Evaluation Software
ADIS16375BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16405BMLZ ADIS16IMU2/PCBZ +5V IMU Evaluation Software
ADIS16407BMLZ ADIS16IMU2/PCBZ +5V IMU Evaluation Software
ADIS16445BMLZ ADIS16IMU2/PCBZ and ADIS1644X/FLEX +3.3V IMU Evaluation Software
ADIS16448BMLZ ADIS16IMU2/PCBZ and ADIS1644X/FLEX +3.3V IMU Evaluation Software
ADIS16460AMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16465-1BMLZ ADIS16IMU4/PCBZ +3.3V IMU Evaluation Software
ADIS16465-2BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16465-3BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16467-1BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16467-2BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16467-3BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16470AMLZ ADIS16470/PCBZ +3.3V IMU Evaluation Software
ADIS16475-1BMLZ ADIS16475-1/PCBZ +3.3V IMU Evaluation Software
ADIS16475-2BMLZ ADIS16475-2/PCBZ +3.3V IMU Evaluation Software
ADIS16475-3BMLZ ADIS16475-3/PCBZ +3.3V IMU Evaluation Software
ADIS16477-1BMLZ ADIS16477-1/PCBZ +3.3V IMU Evaluation Software
ADIS16477-2BMLZ ADIS16477-2/PCBZ +3.3V IMU Evaluation Software
ADIS16477-3BMLZ ADIS16477-3/PCBZ +3.3V IMU Evaluation Software
ADIS16480BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16485BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16488BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16488CMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16490BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16495-1BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16495-2BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16495-3BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16497-1BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16497-2BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16497-3BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16500AMLZ ADIS16500/PCBZ +3.3V IMU Evaluation Software
ADIS16505-1AMLZ ADIS16505-1/PCBZ +3.3V IMU Evaluation Software
ADIS16505-2AMLZ ADIS16505-2/PCBZ +3.3V IMU Evaluation Software
ADIS16505-3AMLZ ADIS16505-3/PCBZ +3.3V IMU Evaluation Software
ADIS16507-1AMLZ ADIS16507-1/PCBZ +3.3V IMU Evaluation Software
ADIS16507-2AMLZ ADIS16507-2/PCBZ +3.3V IMU Evaluation Software
ADIS16507-3AMLZ ADIS16507-3/PCBZ +3.3V IMU Evaluation Software

EVAL-ADIS2 Kit Contents

- EVAL-ADIS2 Evaluation Board

- 6ft Mini USB Cable

- 1.5“ 16-pin IDC Cable

- 12” 16-pin IDC Cable

- M2 Hardware Kit

The EVAL-ADIS2 kit does not include any device-specific breakout board or sensor module.

Minimum PC System Requirements

- Microsoft Windows XP 32-Bit or Later

- Microsoft .NET Framework 3.5

EVAL-ADIS2 Mechanical Drawings

Click here for a more detailed mechanical drawing of the EVAL-ADIS2 evaluation board.

EVAL-ADIS2 J1 (Sensor Interface) Pin Assignments

Legacy Quick-Start Guide

The following guide walks you through setting up and using the EVAL-ADIS2 evaluation kit.

Setting the Sensor Supply

The jumper labeled JP1 provides three power supply options for evaluating our sensors.

- +3.3V

- +5V

- Ext (External Supply)

Use the table below to identify the correct JP1 setting for your sensor.

External Supply Setting In order to use external supply option, remove the header from JP1 and solder the middle post to the hole that has the EXT label on the EVAL-ADIS2.

After soldering the connector, apply the external supply to J3 as shown below.

Connecting a Sensor Breakout Board

All sensor modules require a breakout board to interface with the EVAL-ADIS2. Model-specific breakout boards will only support products that require solder revlow attachment. Generic breakout boards support products that feature an onboard connector and must be purchased in addition to the sensor module.

The following table provides a summary of supported, model-specific breakout boards.

The following table provides a summary of supported, generic breakout boards.

The J1 connector on the EVAL-ADIS2 supports a remote connection to compatible breakout boards using either of the included IDC cables.

The mating connector on the following evaluation boards was designed for a legacy connector solution, but remains compatible with the EVAL-ADIS2.

Pins 13, 14, 15, and 16 on the IDC ribbon cable will remain connected as shown in the image below. warning

Installing the EVAL-ADIS2 USB Driver

Click here to download the latest USB driver for the EVAL-ADIS2.

After downloading the EVAL-ADIS USB Driver file, extract the SDPDrivers.exe file from the zip archive, to a convenient location on your PC. Double click on the extracted file to start the installation process.

Click on Next to accept the default driver location.

The process will involve at least two progress bars that look like the following:

If you encounter this type of message during the process, click on Install to continue with the installation.

Once the installation has completed, click on Finish to complete the process.

Downloading the EVAL-ADIS2 Evaluation Software

Use the table below to find and download the appropriate software for your specific sensor.

Click to display ⇲

Click to hide ⇱

MODEL NUMBER BREAKOUT BOARD JP1 SUPPLY SETTING SOFTWARE PACKAGE
ADIS16133BMLZ ADIS16IMU1/PCBZ +5V IMU Evaluation Software
ADIS16135BMLZ ADIS16IMU1/PCBZ +5V IMU Evaluation Software
ADIS16136BMLZ ADIS16IMU1/PCBZ +5V IMU Evaluation Software
ADIS16137BMLZ ADIS16IMU1/PCBZ +5V IMU Evaluation Software
ADIS16201CCCZ ADIS16201/PCBZ +3.3V IMU Evaluation Software
ADIS16203CCCZ ADIS16203/PCBZ +3.3V IMU Evaluation Software
ADIS16209CCCZ ADIS16209/PCBZ +3.3V IMU Evaluation Software
ADIS16210BMLZ ADIS16ACL1/PCBZ +3.3V IMU Evaluation Software
ADIS16223CMLZ ADIS16ACL2/PCBZ +3.3V ADIS16223 Vibration Evaluation Program
ADIS16227CMLZ ADIS16ACL2/PCBZ +3.3V Vibration Evaluation Program
ADIS16228BMLZ ADIS16ACL1/PCBZ +3.3V Vibration Evaluation Program
ADIS16265BCCZ ADIS16265/PCBZ +5V IMU Evaluation Software
ADIS16334BMLZ ADIS16IMU2/PCBZ and ADIS1644X/FLEX +5V IMU Evaluation Software
ADIS16362BMLZ ADIS16IMU2/PCBZ +5V IMU Evaluation Software
ADIS16364BMLZ ADIS16IMU2/PCBZ +5V IMU Evaluation Software
ADIS16365BMLZ ADIS16IMU2/PCBZ +5V IMU Evaluation Software
ADIS16367BMLZ ADIS16IMU2/PCBZ +5V IMU Evaluation Software
ADIS16375BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16405BMLZ ADIS16IMU2/PCBZ +5V IMU Evaluation Software
ADIS16407BMLZ ADIS16IMU2/PCBZ +5V IMU Evaluation Software
ADIS16445BMLZ ADIS16IMU2/PCBZ and ADIS1644X/FLEX +3.3V IMU Evaluation Software
ADIS16448BMLZ ADIS16IMU2/PCBZ and ADIS1644X/FLEX +3.3V IMU Evaluation Software
ADIS16460AMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16465-1BMLZ ADIS16IMU4/PCBZ +3.3V IMU Evaluation Software
ADIS16465-2BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16465-3BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16467-1BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16467-2BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16467-3BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16470AMLZ ADIS16470/PCBZ +3.3V IMU Evaluation Software
ADIS16475-1BMLZ ADIS16475-1/PCBZ +3.3V IMU Evaluation Software
ADIS16475-2BMLZ ADIS16475-2/PCBZ +3.3V IMU Evaluation Software
ADIS16475-3BMLZ ADIS16475-3/PCBZ +3.3V IMU Evaluation Software
ADIS16477-1BMLZ ADIS16477-1/PCBZ +3.3V IMU Evaluation Software
ADIS16477-2BMLZ ADIS16477-2/PCBZ +3.3V IMU Evaluation Software
ADIS16477-3BMLZ ADIS16477-3/PCBZ +3.3V IMU Evaluation Software
ADIS16480BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16485BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16488BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16488CMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16490BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16495-1BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16495-2BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16495-3BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16497-1BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16497-2BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16497-3BMLZ ADIS16IMU1/PCBZ +3.3V IMU Evaluation Software
ADIS16500AMLZ ADIS16500/PCBZ +3.3V IMU Evaluation Software
ADIS16505-1AMLZ ADIS16505-1/PCBZ +3.3V IMU Evaluation Software
ADIS16505-2AMLZ ADIS16505-2/PCBZ +3.3V IMU Evaluation Software
ADIS16505-3AMLZ ADIS16505-3/PCBZ +3.3V IMU Evaluation Software
ADIS16507-1AMLZ ADIS16507-1/PCBZ +3.3V IMU Evaluation Software
ADIS16507-2AMLZ ADIS16507-2/PCBZ +3.3V IMU Evaluation Software
ADIS16507-3AMLZ ADIS16507-3/PCBZ +3.3V IMU Evaluation Software

Connecting the EVAL-ADIS2 to the Host PC

Connect the EVAL-ADIS2 to any USB 2.0 port on your PC using the included Mini USB cable. LED2 should illuminate indicating that the board is being powered using the PC USB port. LED1 will only illuminate once the SDP Drivers have been installed and the board has successfully enumated in Windows.

LED1 may take up to 10 seconds to illuminate.

Step #7: Start Evaluation Software

Double click on the executable file to launch the application software.

IMU Evaluation Software

Please visit the IMU Evaluation Software Wiki Guide to get some basic operational instructions.

Coming soon: Update to include latest version

Vibration Evaluation Software

Please visit the Vibration Evaluation Software Wiki Guide to get some basic operational instructions.

Development Support

No official support Limited, please feel free to try these examples out.

resources/eval/user-guides/inertial-mems/evaluation-systems/eval-adis2.1613523133.txt.gz · Last modified: 17 Feb 2021 01:52 by Juan Chong