Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:inertial-mems:evaluation-systems:eval-adis-fx3-eval-user-guide [15 Dec 2020 18:37] – Fixed English Juan Chong | resources:eval:user-guides:inertial-mems:evaluation-systems:eval-adis-fx3-eval-user-guide [17 Feb 2021 03:31] (current) – Added links to the EVAL-ADIS-FX3 product page Juan Chong |
---|
====== iSensor Eval GUI User Guide ====== | ====== iSensor Eval GUI User Guide ====== |
| |
<note warning>This guide assumes that you've connected your IMU to the EVAL-ADIS-FX3 and that the Eval GUI software was able to verify communication with your IMU successfully. We recommend checking out the [[resources:eval:user-guides:inertial-mems:evaluation-systems:eval-adis-fx3-setup-troubleshooting|Setup and Troubleshooting]] guide before continuing with the Eval GUI user guide. </note> | <note warning>This guide assumes that you've connected your IMU to the [[adi>EVAL-ADIS-FX3|EVAL-ADIS-FX3]] and that the Eval GUI software was able to verify communication with your IMU successfully. We recommend checking out the [[resources:eval:user-guides:inertial-mems:evaluation-systems:eval-adis-fx3-setup-troubleshooting|Setup and Troubleshooting]] guide before continuing with the Eval GUI user guide. </note> |
| |
===== Eval GUI Main Window ===== | ===== Eval GUI Main Window ===== |
| |
The Eval GUI Main Window brings together many functions, utilities, and subroutines useful when working with the EVAL-ADIS-FX3 and ADI inertial sensors. The image below summarizes the buttons, menus, and tabs available on the main window. | The Eval GUI Main Window brings together many functions, utilities, and subroutines useful when working with the [[adi>EVAL-ADIS-FX3|EVAL-ADIS-FX3]] and ADI inertial sensors. The image below summarizes the buttons, menus, and tabs available on the main window. |
| |
{{:resources:eval:user-guides:inertial-mems:evaluation-systems:main_screen_sections.jpg|}} | {{:resources:eval:user-guides:inertial-mems:evaluation-systems:main_screen_sections.jpg|}} |
| |
- **Reboot FX3** - This button commands the EVAL-ADIS-FX3 to reboot, forcing USB re-enumeration and powering off the sensor supply (if powered through USB). | - **Reboot FX3** - This button commands the [[adi>EVAL-ADIS-FX3|EVAL-ADIS-FX3]] to reboot, forcing USB re-enumeration and powering off the sensor supply (if powered through USB). |
- **FX3 Board Info** - This button displays information describing the EVAL-ADIS-FX3 hardware and firmware and the active FX3Api version, build date and commit information. | - **FX3 Board Info** - This button displays information describing the [[adi>EVAL-ADIS-FX3|EVAL-ADIS-FX3]] hardware and firmware and the active FX3Api version, build date and commit information. |
- **Select DUT Type** - This button calls the DUT Type Selection window, allowing you to quickly change the active device type configuration. Click [[resources:eval:user-guides:inertial-mems:evaluation-systems:eval-adis-fx3-setup-troubleshooting#connecting_to_the_fx3_board|here]] for more information. | - **Select DUT Type** - This button calls the DUT Type Selection window, allowing you to quickly change the active device type configuration. Click [[resources:eval:user-guides:inertial-mems:evaluation-systems:eval-adis-fx3-setup-troubleshooting#connecting_to_the_fx3_board|here]] for more information. |
- **Manual DUT Config** - This button calls the Manual DUT Configuration window. This window allows you to customize the communication protocol settings, sensor supply, active register map, GUI color scheme, and many other features. Click here for a detailed guide on using this window. | - **Manual DUT Config** - This button calls the Manual DUT Configuration window. This window allows you to customize the communication protocol settings, sensor supply, active register map, GUI color scheme, and many other features. Click here for a detailed guide on using this window. |
- **Check DUT Connection** - This button will execute a series of SPI transactions that attempt to validate the sensor's SPI configuration settings and connections. | - **Check DUT Connection** - This button will execute a series of SPI transactions that attempt to validate the sensor's SPI configuration settings and connections. |
- **FX3/DUT Status** - This section displays the FX3 status, sensor status, sensor supply status, and the active device type. | - **FX3/DUT Status** - This section displays the FX3 status, sensor status, sensor supply status, and the active device type. |
- **Evaluation GUI Functions** - These tabs group the EVAL-ADIS-FX3's capabilities into different sections. Many of these capabilities are described in detail below. | - **Evaluation GUI Functions** - These tabs group the [[adi>EVAL-ADIS-FX3|EVAL-ADIS-FX3]]'s capabilities into different sections. Many of these capabilities are described in detail below. |
- ** Evaluation GUI Main Window** - This section of the GUI will update as different tabs are selected. | - ** Evaluation GUI Main Window** - This section of the GUI will update as different tabs are selected. |
- **Evaluation GUI Metadata** - This section displays the Evaluation GUI version and active register map. | - **Evaluation GUI Metadata** - This section displays the Evaluation GUI version and active register map. |
{{:resources:eval:user-guides:inertial-mems:evaluation-systems:read_registers.png}} | {{:resources:eval:user-guides:inertial-mems:evaluation-systems:read_registers.png}} |
| |
<note important>The Eval GUI will automatically append an extra 16-bit SPI transaction (reading 32 bits from the sensor in total) when reading any *_LOW registers (this includes gyroscope, accelerometer, delta angle/velocity, and offset registers). The Eval GUI performs the 16-bit SPI transactions, transmits the data to the PC, and combines the two 16-bit numbers into a single 32-bit number. A single SPI transaction will look like the capture shown below. | <note important>The Eval GUI will automatically append an extra 16-bit SPI transaction (reading 32 bits from the sensor in total) when reading any *_LOW registers (this includes gyroscope, accelerometer, delta angle/velocity, and offset registers where applicable). The Eval GUI performs the 16-bit SPI transactions, transmits the data to the PC, and combines the two 16-bit numbers into a single 32-bit number. A single SPI transaction will look like the capture shown below. |
| |
{{ :resources:eval:user-guides:inertial-mems:evaluation-systems:spi_32bit.jpg |}} | {{ :resources:eval:user-guides:inertial-mems:evaluation-systems:spi_32bit.jpg |}} |
{{:resources:eval:user-guides:inertial-mems:evaluation-systems:add_stream_registers.gif|}} | {{:resources:eval:user-guides:inertial-mems:evaluation-systems:add_stream_registers.gif|}} |
| |
Setting the "DR Active" check box configures the EVAL-ADIS-FX3 to wait for a data ready signal before initiating a SPI transfer. Data captures may be performed without data ready synchronization, but this configuration is not recommended since invalid data may be read from the IMU. The images below show the differences between data captures performed with and without "DR Active" enabled. | Setting the "DR Active" check box configures the [[adi>EVAL-ADIS-FX3|EVAL-ADIS-FX3]] to wait for a data ready signal before initiating a SPI transfer. Data captures may be performed without data ready synchronization, but this configuration is not recommended since invalid data may be read from the IMU. The images below show the differences between data captures performed with and without "DR Active" enabled. |
| |
{{:resources:eval:user-guides:inertial-mems:evaluation-systems:dr_active_inactive.jpg|}} | {{:resources:eval:user-guides:inertial-mems:evaluation-systems:dr_active_inactive.jpg|}} |