This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:inertial-mems:evaluation-systems:eval-adis-fx3-eval-user-guide [15 Dec 2020 18:31] – Fixed formatting Juan Chong | resources:eval:user-guides:inertial-mems:evaluation-systems:eval-adis-fx3-eval-user-guide [17 Feb 2021 03:31] (current) – Added links to the EVAL-ADIS-FX3 product page Juan Chong | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== iSensor Eval GUI User Guide ====== | ====== iSensor Eval GUI User Guide ====== | ||
- | < | + | < |
===== Eval GUI Main Window ===== | ===== Eval GUI Main Window ===== | ||
- | The Eval GUI Main Window brings together many functions, utilities, and subroutines useful when working with the EVAL-ADIS-FX3 and ADI inertial sensors. The image below summarizes the buttons, menus, and tabs available on the main window. | + | The Eval GUI Main Window brings together many functions, utilities, and subroutines useful when working with the [[adi>EVAL-ADIS-FX3|EVAL-ADIS-FX3]] |
{{: | {{: | ||
- | - **Reboot FX3** - This button commands the EVAL-ADIS-FX3 to reboot, forcing USB re-enumeration and powering off the sensor supply (if powered through USB). | + | - **Reboot FX3** - This button commands the [[adi>EVAL-ADIS-FX3|EVAL-ADIS-FX3]] |
- | - **FX3 Board Info** - This button displays information describing the EVAL-ADIS-FX3 hardware and firmware and the active FX3Api version, build date and commit information. | + | - **FX3 Board Info** - This button displays information describing the [[adi> |
- **Select DUT Type** - This button calls the DUT Type Selection window, allowing you to quickly change the active device type configuration. Click [[resources: | - **Select DUT Type** - This button calls the DUT Type Selection window, allowing you to quickly change the active device type configuration. Click [[resources: | ||
- **Manual DUT Config** - This button calls the Manual DUT Configuration window. This window allows you to customize the communication protocol settings, sensor supply, active register map, GUI color scheme, and many other features. Click here for a detailed guide on using this window. | - **Manual DUT Config** - This button calls the Manual DUT Configuration window. This window allows you to customize the communication protocol settings, sensor supply, active register map, GUI color scheme, and many other features. Click here for a detailed guide on using this window. | ||
Line 16: | Line 16: | ||
- **Check DUT Connection** - This button will execute a series of SPI transactions that attempt to validate the sensor' | - **Check DUT Connection** - This button will execute a series of SPI transactions that attempt to validate the sensor' | ||
- **FX3/DUT Status** - This section displays the FX3 status, sensor status, sensor supply status, and the active device type. | - **FX3/DUT Status** - This section displays the FX3 status, sensor status, sensor supply status, and the active device type. | ||
- | - **Evaluation GUI Functions** - These tabs group the EVAL-ADIS-FX3' | + | - **Evaluation GUI Functions** - These tabs group the [[adi>EVAL-ADIS-FX3|EVAL-ADIS-FX3]]'s capabilities into different sections. Many of these capabilities are described in detail below. |
- ** Evaluation GUI Main Window** - This section of the GUI will update as different tabs are selected. | - ** Evaluation GUI Main Window** - This section of the GUI will update as different tabs are selected. | ||
- **Evaluation GUI Metadata** - This section displays the Evaluation GUI version and active register map. | - **Evaluation GUI Metadata** - This section displays the Evaluation GUI version and active register map. | ||
Line 33: | Line 33: | ||
{{: | {{: | ||
- | <note important> | + | <note important> |
{{ : | {{ : | ||
Line 63: | Line 63: | ||
{{: | {{: | ||
- | Setting the "DR Active" | + | Setting the "DR Active" |
{{: | {{: |