Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:inertial-mems:accelerometers:adxl367 [09 Sep 2021 17:40] – Pablo del Corro | resources:eval:user-guides:inertial-mems:accelerometers:adxl367 [14 Apr 2023 18:34] (current) – [Evaluating the ADXL367] Pablo del Corro |
---|
//Useful links:\\ | //Useful links:\\ |
ADXL367 [[ADI>adxl367|product page]] | [[ADI>media/en/technical-documentation/data-sheets/ADXL367.pdf|datasheet]]. \\ | ADXL367 [[ADI>adxl367|product page]] | [[ADI>media/en/technical-documentation/data-sheets/ADXL367.pdf|datasheet]]. \\ |
| ADXL367 pedometer algorithm implementation with Arduino Nano 33 BLE: {{ :resources:eval:user-guides:inertial-mems:accelerometers:adxl367_pedometer.zip |}} |
// \\ | // \\ |
| |
=== EVAL-ADXL367Z: === | === EVAL-ADXL367Z: === |
This is a small footprint PCB that consist of the ADXL367 and pin headers. | This is a small footprint PCB that consist of the ADXL367 and pin headers. |
| {{ :resources:eval:user-guides:inertial-mems:accelerometers:eval-adxl367z_photo.jpg?nolink&400 |}} |
=== EVAL-ADXL367-SDP: === | === EVAL-ADXL367-SDP: === |
ADXL367 evaluation system based on ADI's [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/SDP-B]|SDP-B evaluation board]]. This a plug and play solution that allows testing of all ADXL367 features. Drivers to install the LabView based GUI are provided. | ADXL367 evaluation system based on ADI's [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/SDP-B]|SDP-B evaluation board]]. This a plug and play solution that allows testing of all ADXL367 features. Drivers to install the LabView based GUI are provided. |
| {{ :resources:eval:user-guides:inertial-mems:accelerometers:eval-adxl367-sdp_photo.jpg?nolink |}} |
| |
* The EVAL-ADXL367-SDP drivers can be downloaded from the following GitHub site: [[https://github.com/bbearssADI/ADXL367-Evaluation-Software|EVAL-ADXL367-SDP drivers]]. | * The EVAL-ADXL367-SDP drivers can be downloaded from the following GitHub site: [[https://github.com/bbearssADI/ADXL367-Evaluation-Software|EVAL-ADXL367-SDP drivers]]. |
| |
* The EVAL-ADXL367-SDP User Guide wiki:[[resources:eval:user-guides:inertial-mems:accelerometers:adxl367:eval-adxl367-sdp|EVAL-ADXL367-SDP User Guide]] | * The EVAL-ADXL367-SDP User Guide: :[[:resources:eval:user-guides:inertial-mems:accelerometers:adxl367:eval-adxl367-sdp|EVAL-ADXL367-SDP wiki]] |
| |