This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:eval:user-guides:inertial-mems:accelerometers:adxl367 [09 Sep 2021 17:36] – created Pablo del Corro | resources:eval:user-guides:inertial-mems:accelerometers:adxl367 [14 Apr 2023 18:34] (current) – [Evaluating the ADXL367] Pablo del Corro | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ===== Evaluating the ADXL367 ====== | + | ====== Evaluating the ADXL367 ====== |
//Useful links: | //Useful links: | ||
ADXL367 [[ADI> | ADXL367 [[ADI> | ||
+ | ADXL367 pedometer algorithm implementation with Arduino Nano 33 BLE: {{ : | ||
// \\ | // \\ | ||
- | ==== ADXL367 Quick Start: | + | ===== ADXL367 Quick Start: ===== |
+ | | ||
The following wiki page goal is to help new users and ADXL362 users to have an easy start testing and prototyping the ADXL367. | The following wiki page goal is to help new users and ADXL362 users to have an easy start testing and prototyping the ADXL367. | ||
* [[resources/ | * [[resources/ | ||
- | === Evaluation boards ordering guide: === | + | ==== Evaluation boards ordering guide: ==== |
- | * **EVAL-ADXL367Z: | + | |
- | * **EVAL-ADXL367-SDP: | + | |
+ | === EVAL-ADXL367Z: | ||
+ | This is a small footprint PCB that consist of the ADXL367 and pin headers. | ||
+ | {{ : | ||
+ | === EVAL-ADXL367-SDP: | ||
+ | | ||
+ | {{ : | ||
- | ==== EVAL-ADXL367-SDP: | + | * The EVAL-ADXL367-SDP drivers can be downloaded from the following GitHub site: [[https:// |
- | The EVAL-ADXL367-SDP drivers can be downloaded from the following GitHub site: | + | |
- | [[https:// | + | |
- | The EVAL-ADXL367-SDP User Guide wiki: | + | * The EVAL-ADXL367-SDP User Guide: |
- | [[resources: | + | |