Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:inertial-mems:accelerometers:adxl362:eval-adxl362z-db [01 Mar 2013 00:06] – [Firmware User Guides] Nitzan Gadishresources:eval:user-guides:inertial-mems:accelerometers:adxl362:eval-adxl362z-db [25 Jan 2021 05:22] (current) – update renesas links after their web site update Robin Getz
Line 30: Line 30:
 ==== Drivers ==== ==== Drivers ====
  
-Download and install these drivers to connect the board to your PC, then follow these **[[resources:eval:user-guides:inertial-mems:evalsystem:installdrivers|written instructions]]** or **[[http://www.analog.com/static/imported-files/eval_boards/InstallDrivers.zip|video instructions]]** for installation.\\+Download and install these drivers to connect the board to your PC, then follow these **[[resources:eval:user-guides:inertial-mems:evalsystem:installdrivers|written instructions]]** or **[[adi>static/imported-files/eval_boards/InstallDrivers.zip|video instructions]]** for installation.\\
 {{:resources:eval:user-guides:inertial-mems:accelerometers:adxl362:vcomusbdriver_v2040a_32bit.zip|32-bit}} or {{:resources:eval:user-guides:inertial-mems:accelerometers:adxl362:vcomusbdriver_v2040a_64bit.zip|64-bit}} {{:resources:eval:user-guides:inertial-mems:accelerometers:adxl362:vcomusbdriver_v2040a_32bit.zip|32-bit}} or {{:resources:eval:user-guides:inertial-mems:accelerometers:adxl362:vcomusbdriver_v2040a_64bit.zip|64-bit}}
 ==== Programming Environment ==== ==== Programming Environment ====
Line 36: Line 36:
 \\ \\
 [[http://www.renesas.eu/products/tools/evaluation_software/downloads.jsp]]  (Global site)\\ [[http://www.renesas.eu/products/tools/evaluation_software/downloads.jsp]]  (Global site)\\
-[[http://am.renesas.com/products/tools/evaluation_software/downloads.jsp]]  (US site)+[[https://www.renesas.com/us/en/design-support/software-and-tool]]  (US site)
  
 ====== Getting Started ====== ====== Getting Started ======
Line 47: Line 47:
 </wrap> </wrap>
   - Power the board.\\ <wrap>   - Power the board.\\ <wrap>
-- This board ships pre-programmed with the MultiDemo firmware that allows is to be used as a motion switch, data logger, or input to a real-time PC-connected user interface. The motion switch functionality can be used with the coin cell battery alone, without downloading any drivers or connecting to USB. Just insert a CR2450 coin cell batter in the holder on the back of the board, ensure all jumpers and switches are in the appropriate positions, and turn the board on. \\+- This board ships pre-programmed with the MultiDemo firmware that allows is to be used as a motion switch, data logger, or input to a real-time PC-connected user interface. The motion switch functionality can be used with the coin cell battery alone, without downloading any drivers or connecting to USB. Just insert a CR2450 coin cell batter in the holder on the back of the board, ensure all jumpers and switches are in the appropriate positions, and turn the board on. (this shows the back side of the board with the battery orientation - positive side of battery facing out{{:resources:eval:user-guides:inertial-mems:accelerometers:adxl362:adxl326_battery.jpg?300|}}) 
 +\\
 - To use the data logger or real-time evaluation functionality, you will need to install drivers and other files. Proceed to the next step for instructions.\\ - To use the data logger or real-time evaluation functionality, you will need to install drivers and other files. Proceed to the next step for instructions.\\
 </wrap> </wrap>
Line 56: Line 57:
 Analog Devices has developed firmware for implementing the following functions via the EVAL-ADXL362Z-DB: Analog Devices has developed firmware for implementing the following functions via the EVAL-ADXL362Z-DB:
  
-  * **Datalogger and GUI (includes real-time data viewer and tilt sensor)**: logs data onto (supplied) microSD card. {{:resources:eval:user-guides:inertial-mems:accelerometers:adxl362:adxl362db_multidemo.zip|ZIP}} //(includes .hex firmware and .exe GUI)//+  * **Datalogger and GUI (includes real-time data viewer and tilt sensor)**: logs data onto (supplied) microSD card.  //(includes .hex firmware and .exe GUI)//[[ftp://ftp.analog.com/pub/iMEMS_Sensor_Eval/EVAL-ADXL362Z-DB/]]
   * **Tilt Sensor**: shows tilt measurement on E-Ink display. {{:resources:eval:user-guides:inertial-mems:accelerometers:adxl362:adxl362db_inclinometer.zip|HEX}} | {{:resources:eval:user-guides:inertial-mems:accelerometers:adxl362:adxl362db_inclinometer_proj.zip|Source Code}}    * **Tilt Sensor**: shows tilt measurement on E-Ink display. {{:resources:eval:user-guides:inertial-mems:accelerometers:adxl362:adxl362db_inclinometer.zip|HEX}} | {{:resources:eval:user-guides:inertial-mems:accelerometers:adxl362:adxl362db_inclinometer_proj.zip|Source Code}} 
   * **Ultralow Power Motion switch**: turns display icons on or off based on presence or absence of motion. {{:resources:eval:user-guides:inertial-mems:accelerometers:adxl362:adxl362db_motionswitch.zip|HEX}} | {{:resources:eval:user-guides:inertial-mems:accelerometers:adxl362:adxl362db_motionswitch_proj.zip|Source Code}}    * **Ultralow Power Motion switch**: turns display icons on or off based on presence or absence of motion. {{:resources:eval:user-guides:inertial-mems:accelerometers:adxl362:adxl362db_motionswitch.zip|HEX}} | {{:resources:eval:user-guides:inertial-mems:accelerometers:adxl362:adxl362db_motionswitch_proj.zip|Source Code}} 
   * Pedometer & fall detector coming soon   * Pedometer & fall detector coming soon
- 
 ===== Reconfiguring the Board ===== ===== Reconfiguring the Board =====
  
Line 92: Line 92:
 ===== Multi-Demo Firmware ===== ===== Multi-Demo Firmware =====
  
 +The Multi-Demo firmware is pre-programmed onto the Datalogger Board, so out of the box, the behavior of the board will match the description in this section. This firmware may always be re-programmed onto the board using [[#Reconfiguring_The_Board|these instructions]] and the .hex file posted [[#Firmware_Options|here]].
 + 
 To use the MultiDemo firmware: To use the MultiDemo firmware:
-On power-up, the board should be a motion switch: he should be able to see the numbers come on with motion and turn off when there is no motion. +  - On power-up, the board behaves as a motion switch: the entire display lights up when the board is moved. When the board is still for a few secondsmost icons turn off and only the logospower and battery icons remain on. Initial power up state: {{ :resources:eval:user-guides:inertial-mems:accelerometers:adxl362:poweridle.jpg?300 |}}  After movementall of the logos, digits, power and battery icons will light: {{ :resources:eval:user-guides:inertial-mems:accelerometers:adxl362:poweractive.jpg?300 |}} 
-When you connect to the PCopen up the LabView GUI, and connect to the correct COM port, the board display should say "PC". At this point the GUI *should* be functional+  - To log data, at any time, insert the microSD card into the slot and press the SW3 button in the top right-hand corner of the board. The word "LOg" will be shown on the display. The hand iconif present, indicates a logging error. Generally this appears when the microSD card is not inserted fully into the slotIf no hand icon lights up, data logging begins when the word "LOg" is shownand continues until power is removed from the board. 
-If you want to log data, insert an SD card. Press SW3 and the display will say "LOg" (not L09but looks the same :) ) and the board will begin receiving data. +  To download logged data onto a computer, use the GUI provided hereInstallation of the GUI is straightforward:  
-To stop logging, turn the board off+  - The GUI also enables adjustment of output data rate and measurement range for data logging.  
-To download logged data, use the GUI.+  - 
 ===== Motion Switch ===== ===== Motion Switch =====
  
Line 126: Line 128:
  
 Note that tilt measurement is, in general, a slow measurement. This is because at any given moment, the motion of your hand, for example, could be producing acceleration that would interfere with the tilt measurement. If we average the total acceleration measurement over time, we can get rid of the transient, or AC, effects, such as those due to your hand moving, and we are left only with long-term, or DC, effects -- in this case, gravity. So for best results, tilt slowly and wait for the display to refresh. Note that tilt measurement is, in general, a slow measurement. This is because at any given moment, the motion of your hand, for example, could be producing acceleration that would interfere with the tilt measurement. If we average the total acceleration measurement over time, we can get rid of the transient, or AC, effects, such as those due to your hand moving, and we are left only with long-term, or DC, effects -- in this case, gravity. So for best results, tilt slowly and wait for the display to refresh.
 +
 +===== Write your own software =====
 +Talking to the development board can be done using your own program with the following commands:
 +
 +Baud rate: 153600 8N1
 +
 +Commands:
 +0xAA  - Enable PC control, the board should respond (500+ ms) 0x55 and Eink display will show "PC"
 +
 +0xB1 to start collecting data
 +    Start collection can be augmented with additional commands which specify different modes
 +       
 +    0xB1 0x0L 0x00 0xGS 0xN2
 +    Where L is the length: 1 for 8-bit; 0 for 12-bit
 +    G is the maximum G: 1 - 2G; 5 - 4G; 9 - 8G
 +    S is the sampling rate: 0-12.5hz;1-25hz;2-50hz;3-100hz;4-200hz;5-400hz
 +    N is the filtering: 0-Normal; 1-Low Noise; 2-Ultra low noise
 +    
 +    EG: 0xB1 0x00 0x00 0x15 0x02   would be start, 12-bit samples, 2G max, 400hz sampling, normal noise mode.    
 +    
 +0xB2 to end collecting data
 +
 +
 +Data is transmitted 16-bits for each direction, 2's compliment, little-endian, in groups of XYZ (48-bits at a time, or 6 bytes).
 +The first block of data will be 8-bytes and can be discarded.
 +
resources/eval/user-guides/inertial-mems/accelerometers/adxl362/eval-adxl362z-db.1362092791.txt.gz · Last modified: 01 Mar 2013 00:06 by Nitzan Gadish