This is an old revision of the document!
ADXL362 Datalogger & Development Board
Thanks for visiting!
This page is UNDER CONSTRUCTION.
Resources
Kit Contents
1 x ADXL362 Datalogger / Development Board
1 x MicroSD card with USB reader
1 x USB cable
1 x E-Ink electronic paper display
1 x Piece of double-sided foam tape
Not Included
1 x CR2450 coin cell battery, required only if stand-alone operation is desired. Full functionality of the board is availabe using USB power.
Design and Integration Files
Programming Environment
Getting Started
Using the Board
Firmware Options
Analog Devices has developed firmware for implementing the following functions via the EVAL-ADXL362Z-DB:
Reconfiguring the Board
The EVAL-ADXL362Z-DB firmware can be rewritten using the Renesas Flash Programmer (click here for download links). Instructions for rewriting the firmware are as follows:
Download the desired firmware .hex file from
here. Save it in a known location.
Set jumpers: J6, J7, J8, and J9 (between the
USB connector and the switch) to the 1-2 position. Set jumper J2 (near the display connector) to the 2-3 position for
USB power.
We know the jumpers are a pain and we apologize in advance.
Jumper | Position | |
J2 | 1 | 2 | 3 |
J6 | 1 | 2 | 3 |
J7 | 1 | 2 | 3 |
J8 | 1 | 2 | 3 |
J9 | 1 | 2 | 3 |
Plug the
USB cable in to the computer and to the
USB port on the board.
Launch the
Renesas Flash Programmer V1.03 (download
here)
Choose “Create new workspace”
Input RL78/G13 in the Filter text box. Select the entry with Device Name “R5F100LJ”, and enter a workspace name. Click Next.
In the “Select Communication Interface” screen, use the pull-down menu next to “Select Tool” to choose the appropriate COM port for the board. Click Next.
On the “Setting Power Supply” screen, leave the default settings and click Next.
On the “Setting Oscillator” screen, and select the corresponding COM port for the board. Click Next.
The “Information Settings” screen shows a summary of inputted settings. Click Complete.
The Workspace is now set up. Next to “User/Data area”, browse to the desired .hex file (that you downloaded and saved in step 1.)
Click “Start”.
When flashing is complete, disconnect the
USB cable (to power the board off) and set jumpers J6 - J9 back to the 2-3 position. Leave J2 where it is to
USB power, or move it to the 1-2 position to power the board from the coin cell.
Jumper | Position | |
J2 | 1 | 2 | 3 |
J6 | 1 | 2 | 3 |
J7 | 1 | 2 | 3 |
J8 | 1 | 2 | 3 |
J9 | 1 | 2 | 3 |
Reconnect the
USB cable OR plug in the battery and turn on the switch to begin using the board.