This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:inertial-mems:accelerometers:adxl362:eval-adxl362z-db [18 Jan 2013 03:18] – [Drivers] Nitzan Gadish | resources:eval:user-guides:inertial-mems:accelerometers:adxl362:eval-adxl362z-db [03 Jan 2021 22:04] – fix links Robin Getz | ||
---|---|---|---|
Line 30: | Line 30: | ||
==== Drivers ==== | ==== Drivers ==== | ||
- | Download and install these drivers to connect the board to your PC, then follow these **[[resources: | + | Download and install these drivers to connect the board to your PC, then follow these **[[resources: |
{{: | {{: | ||
==== Programming Environment ==== | ==== Programming Environment ==== | ||
Line 47: | Line 47: | ||
</ | </ | ||
- Power the board.\\ < | - Power the board.\\ < | ||
- | - This board ships pre-programmed with the MultiDemo firmware that allows is to be used as a motion switch, data logger, or input to a real-time PC-connected user interface. The motion switch functionality can be used with the coin cell battery alone, without downloading any drivers or connecting to USB. Just insert a CR2450 coin cell batter in the holder on the back of the board, ensure all jumpers and switches are in the appropriate positions, and turn the board on. \\ | + | - This board ships pre-programmed with the MultiDemo firmware that allows is to be used as a motion switch, data logger, or input to a real-time PC-connected user interface. The motion switch functionality can be used with the coin cell battery alone, without downloading any drivers or connecting to USB. Just insert a CR2450 coin cell batter in the holder on the back of the board, ensure all jumpers and switches are in the appropriate positions, and turn the board on. (this shows the back side of the board with the battery orientation - positive side of battery facing out{{: |
+ | \\ | ||
- To use the data logger or real-time evaluation functionality, | - To use the data logger or real-time evaluation functionality, | ||
</ | </ | ||
Line 56: | Line 57: | ||
Analog Devices has developed firmware for implementing the following functions via the EVAL-ADXL362Z-DB: | Analog Devices has developed firmware for implementing the following functions via the EVAL-ADXL362Z-DB: | ||
- | * **Datalogger and GUI (includes real-time data viewer and tilt sensor)**: logs data onto (supplied) microSD card. {{: | + | * **Datalogger and GUI (includes real-time data viewer and tilt sensor)**: logs data onto (supplied) microSD card. //(includes .hex firmware and .exe GUI)//[[ftp:// |
* **Tilt Sensor**: shows tilt measurement on E-Ink display. {{: | * **Tilt Sensor**: shows tilt measurement on E-Ink display. {{: | ||
* **Ultralow Power Motion switch**: turns display icons on or off based on presence or absence of motion. {{: | * **Ultralow Power Motion switch**: turns display icons on or off based on presence or absence of motion. {{: | ||
* Pedometer & fall detector coming soon | * Pedometer & fall detector coming soon | ||
- | |||
===== Reconfiguring the Board ===== | ===== Reconfiguring the Board ===== | ||
Line 90: | Line 90: | ||
This section describes operation of the firmware options provided by Analog Devices for this development board. To download firmware, click [[# | This section describes operation of the firmware options provided by Analog Devices for this development board. To download firmware, click [[# | ||
+ | ===== Multi-Demo Firmware ===== | ||
+ | |||
+ | The Multi-Demo firmware is pre-programmed onto the Datalogger Board, so out of the box, the behavior of the board will match the description in this section. This firmware may always be re-programmed onto the board using [[# | ||
+ | |||
+ | To use the MultiDemo firmware: | ||
+ | - On power-up, the board behaves as a motion switch: the entire display lights up when the board is moved. When the board is still for a few seconds, most icons turn off and only the logos, power and battery icons remain on. Initial power up state: {{ : | ||
+ | - To log data, at any time, insert the microSD card into the slot and press the SW3 button in the top right-hand corner of the board. The word " | ||
+ | - To download logged data onto a computer, use the GUI provided here. Installation of the GUI is straightforward: | ||
+ | - The GUI also enables adjustment of output data rate and measurement range for data logging. | ||
+ | - | ||
===== Motion Switch ===== | ===== Motion Switch ===== | ||
Line 118: | Line 128: | ||
Note that tilt measurement is, in general, a slow measurement. This is because at any given moment, the motion of your hand, for example, could be producing acceleration that would interfere with the tilt measurement. If we average the total acceleration measurement over time, we can get rid of the transient, or AC, effects, such as those due to your hand moving, and we are left only with long-term, or DC, effects -- in this case, gravity. So for best results, tilt slowly and wait for the display to refresh. | Note that tilt measurement is, in general, a slow measurement. This is because at any given moment, the motion of your hand, for example, could be producing acceleration that would interfere with the tilt measurement. If we average the total acceleration measurement over time, we can get rid of the transient, or AC, effects, such as those due to your hand moving, and we are left only with long-term, or DC, effects -- in this case, gravity. So for best results, tilt slowly and wait for the display to refresh. | ||
+ | |||
+ | ===== Write your own software ===== | ||
+ | Talking to the development board can be done using your own program with the following commands: | ||
+ | |||
+ | Baud rate: 153600 8N1 | ||
+ | |||
+ | Commands: | ||
+ | 0xAA - Enable PC control, the board should respond (500+ ms) 0x55 and Eink display will show " | ||
+ | |||
+ | 0xB1 to start collecting data | ||
+ | Start collection can be augmented with additional commands which specify different modes | ||
+ | |||
+ | 0xB1 0x0L 0x00 0xGS 0xN2 | ||
+ | Where L is the length: 1 for 8-bit; 0 for 12-bit | ||
+ | G is the maximum G: 1 - 2G; 5 - 4G; 9 - 8G | ||
+ | S is the sampling rate: 0-12.5hz; | ||
+ | N is the filtering: 0-Normal; 1-Low Noise; 2-Ultra low noise | ||
+ | | ||
+ | EG: 0xB1 0x00 0x00 0x15 0x02 would be start, 12-bit samples, 2G max, 400hz sampling, normal noise mode. | ||
+ | | ||
+ | 0xB2 to end collecting data | ||
+ | |||
+ | |||
+ | Data is transmitted 16-bits for each direction, 2's compliment, little-endian, | ||
+ | The first block of data will be 8-bytes and can be discarded. | ||
+ |