This is an old revision of the document!
The ADXL314 is a 3-axis accelerometer that provides low power consumption and high-resolution measurement up to ±200 g. The digital output data is formatted as 16-bit, twos complement data and is accessible through a SPI (3- or 4-wire) or I2C digital interface.
The EVAL-ADXL314-SDP drivers and User Guide can be downloaded from the following ftp site: EVAL-ADXLx-SDP Eval Platform.
The EVAL-ADXL314-SDP User Guide wiki: EVAL-ADXL314-SDP User Guide