This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-cog-ad4050lz:software:sensors [11 Aug 2017 11:55] – [General Description/Overview] Pranit Jadhav | resources:eval:user-guides:eval-cog-ad4050lz:software:sensors [12 Aug 2017 09:19] (current) – Pranit Jadhav | ||
---|---|---|---|
Line 24: | Line 24: | ||
===== Downloading the Sensor Software Pack ===== | ===== Downloading the Sensor Software Pack ===== | ||
- | The software pack can be downloaded in several | + | The software pack can be downloaded in following |
- Downloaded via the tools program | - Downloaded via the tools program | ||
* It is **recommended** to download the Sensor software pack through from the tools program you are using. | * It is **recommended** to download the Sensor software pack through from the tools program you are using. | ||
Line 31: | Line 31: | ||
| | ||
<WRAP center round download 80%> | <WRAP center round download 80%> | ||
- | Download the Sensor Software Pack to your computer. | + | Download the Sensor Software Pack.\\ |
- | ADD LINK HERE SENSOR SOFTWARE PACK | + | [[http:// |
</ | </ | ||
Line 39: | Line 39: | ||
// End of Document // | // End of Document // | ||
+ | |||
+ | |