This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-cog-ad4050lz:software:sensors [11 Aug 2017 10:15] – Pranit Jadhav | resources:eval:user-guides:eval-cog-ad4050lz:software:sensors [12 Aug 2017 09:19] (current) – Pranit Jadhav | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Sensor Application Software Packs and Drivers ====== | ====== Sensor Application Software Packs and Drivers ====== | ||
===== General Description/ | ===== General Description/ | ||
- | Sensor software pack contains sensor software components. Sensor components are based on the sensor classes which abstract the functionality across sensor types. The Sensors software pack provides access to all the necessary add-on module digital drivers that attach to the [[ADI> | + | Sensor software pack contains sensor software components. Sensor components are based on the sensor classes which abstract the functionality across sensor types. The Sensors software pack provides access to all the necessary add-on module digital drivers that attach to the [[ADI> |
ADI Sensor Software requires CrossCore Embedded Studio 2.6.0 ® , ADuCM4050 Device Family Pack 2.0.0 and EV-COG-AD4050LZ Board Support Package 1.0.0. | ADI Sensor Software requires CrossCore Embedded Studio 2.6.0 ® , ADuCM4050 Device Family Pack 2.0.0 and EV-COG-AD4050LZ Board Support Package 1.0.0. | ||
- | + | ||
- | + | The following application examples and sensor drivers are provided as part of the Sensor software pack: | |
+ | * Accelerometer Demo | ||
+ | * Temperature Sensor Demo | ||
For detailed information regarding the Sensor software pack, please see our complete Sensor software user guide. | For detailed information regarding the Sensor software pack, please see our complete Sensor software user guide. | ||
Line 22: | Line 24: | ||
===== Downloading the Sensor Software Pack ===== | ===== Downloading the Sensor Software Pack ===== | ||
- | The software pack can be downloaded in several | + | The software pack can be downloaded in following |
- Downloaded via the tools program | - Downloaded via the tools program | ||
* It is **recommended** to download the Sensor software pack through from the tools program you are using. | * It is **recommended** to download the Sensor software pack through from the tools program you are using. | ||
Line 29: | Line 31: | ||
| | ||
<WRAP center round download 80%> | <WRAP center round download 80%> | ||
- | Download the Sensor Software Pack to your computer. | + | Download the Sensor Software Pack.\\ |
- | ADD LINK HERE SENSOR SOFTWARE PACK | + | [[http:// |
</ | </ | ||
Line 37: | Line 39: | ||
// End of Document // | // End of Document // | ||
+ | |||
+ | |