This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:eval:user-guides:eval-cog-ad4050lz:software:sensors [10 Jul 2017 08:16] – created Pranit Jadhav | resources:eval:user-guides:eval-cog-ad4050lz:software:sensors [12 Aug 2017 09:19] (current) – Pranit Jadhav | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Sensor Application Software Packs & Drivers ====== | + | ====== Sensor Application Software Packs and Drivers ====== |
+ | ===== General Description/ | ||
+ | Sensor software pack contains sensor software components. Sensor components are based on the sensor classes which abstract the functionality across sensor types. The Sensors software pack provides access to all the necessary add-on module digital drivers that attach to the [[ADI> | ||
+ | ADI Sensor Software requires CrossCore Embedded Studio 2.6.0 ® , ADuCM4050 Device Family Pack 2.0.0 and EV-COG-AD4050LZ Board Support Package 1.0.0. | ||
+ | |||
+ | The following application examples and sensor drivers are provided as part of the Sensor software pack: | ||
+ | * Accelerometer Demo | ||
+ | * Temperature Sensor Demo | ||
+ | |||
+ | For detailed information regarding the Sensor software pack, please see our complete Sensor software user guide. | ||
+ | <WRAP center round help 60%> | ||
+ | |||
+ | ADD LINK HERE Sensor Software Pack Release Notes. | ||
+ | |||
+ | </ | ||
+ | |||
+ | <WRAP center round important 60%> | ||
+ | |||
+ | You **MUST** have this software package installed on your laptop or PC in order to compile, debug, and run the applications for the EC-COG-AD4050LZ platform. | ||
+ | |||
+ | </ | ||
+ | |||
+ | ===== Downloading the Sensor Software Pack ===== | ||
+ | |||
+ | The software pack can be downloaded in following ways. | ||
+ | - Downloaded via the tools program | ||
+ | * It is **recommended** to download the Sensor software pack through from the tools program you are using. | ||
+ | - Downloaded to local directory | ||
+ | * However if you do decide to download the Sensor software pack to your PC/laptop directly, please use the link below, and make sure you save the software pack to the correct local directory for your applications/ | ||
+ | | ||
+ | <WRAP center round download 80%> | ||
+ | Download the Sensor Software Pack.\\ | ||
+ | |||
+ | [[http:// | ||
+ | |||
+ | </ | ||
+ | |||
+ | |||
+ | // End of Document // | ||
+ | |||
+ | |