This shows you the differences between two versions of the page.
Previous revisionNext revision | |||
— | resources:eval:user-guides:eval-cog-ad3029lz:tools:cces_download [12 Aug 2017 07:51] – [CrossCore Embedded Studio Support] Pranit Jadhav | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== CrossCore Embedded Studio Download & Install ====== | ||
+ | This page provides all the necessary steps to get CrossCore Embedded Studio (CCES) software environment up and running on Windows or Linux. | ||
+ | |||
+ | The CCES software development environment for EV-COG-AD3029LZ is based on open source tools, and is maintained by Analog Devices. CCES includes support for DSP (digital signal processing) and ARM Cortex M- and A- devices, and includes the following features and many more: | ||
+ | * Eclipse based IDE | ||
+ | * GNU ARM Embedded Toolchain for Cortex-M core based parts (5-2016-q2-update release) | ||
+ | * OpenOCD with support for ADuCM302x and ADuCM4x50 microcontroller (open source SWD) | ||
+ | * CMSIS Pack files | ||
+ | * Mbed CMSIS-DAP | ||
+ | * J-Link Lite | ||
+ | |||
+ | <note important> | ||
+ | **CrossCore Embedded Studio** is based on **Eclipse**, | ||
+ | </ | ||
+ | |||
+ | ====== Pre-Requisites and Requirements List ====== | ||
+ | |||
+ | There are a few things that you will need for the tools and software to work properly. | ||
+ | * PC or laptop computer | ||
+ | * EV-COG-AD3029LZ hardware | ||
+ | * Micro USB to USB cables | ||
+ | <note important> | ||
+ | * Terminal Program to interface your PC with the EV-COG-AD3029LZ | ||
+ | * [[http:// | ||
+ | * [[https:// | ||
+ | * Or other favorite Terminal program | ||
+ | |||
+ | ====== CrossCore Embedded Studio Download Packages ====== | ||
+ | |||
+ | <WRAP round 100% download> | ||
+ | |||
+ | The EV-COG-AD3029LZ **requires** the use of Crosscore Embedded Studios version **2.6.0 or higher**. | ||
+ | \\ | ||
+ | |||
+ | {{http:// | ||
+ | |||
+ | {{http:// | ||
+ | |||
+ | </ | ||
+ | |||
+ | ==== The following features are available and supported ==== | ||
+ | * Compilation using the GNU ARM Embedded toolchain for the ADuCM302x and ADuCM4x50 ARM Cortex-M cores. | ||
+ | * Debugging ADuCM302x and ADuCM4x50 via the IDE with GDB/ | ||
+ | * Development and debugging of bare-metal applications on the ADuCM302x and ADuCM4x50 ARM Cortex-M core. | ||
+ | |||
+ | ==== The following features are only supported via the Windows version ==== | ||
+ | * Use of CrossCore Embedded Studio Add-Ins other than the Linux Add-In | ||
+ | * Debugging an Application using the CrossCore Debugger (TPSDK) | ||
+ | |||
+ | ====== CrossCore Embedded Studio Installer Instructions ====== | ||
+ | |||
+ | It is best that you save all the files/ | ||
+ | |||
+ | ===== Installing CrossCore Embedded Studio on Windows ===== | ||
+ | |||
+ | * To install CrossCore Embedded Studio, double-click ADI_CrossCoreEmbeddedStudio-Rel2.6.0.exe | ||
+ | * The CrossCore Embedded Studio installer will install the mBed windows serial driver. | ||
+ | * It is available separately, if required | ||
+ | * https:// | ||
+ | |||
+ | The executable installs all necessary components to the Analog Devices local directory structure which can be found below. | ||
+ | |||
+ | * CrossCore Embedded Studio installs to **C:\Analog Devices\CrossCore Embedded Studio 2.6.0** | ||
+ | * Eclipse IDE installs to **C:\Analog Devices\CrossCore Embedded Studio 2.6.0\Eclipse** | ||
+ | * GNU ARM Embedded Toolchain for Cortex-M installs to **C:\Analog Devices\CrossCore Embedded Studio 2.6.0\ARM\gcc-arm-embedded** | ||
+ | * OpenOCD installs to **C:\Analog Devices\CrossCore Embedded Studio 2.6.0\ARM\openocd\bin** | ||
+ | * CMSIS Pack files are installed to **C:\Analog Devices\CrossCore Embedded Studio 2.5.1\ARM\packs** | ||
+ | |||
+ | ===== Installing CrossCore Embedded Studio on Linux ===== | ||
+ | |||
+ | * To install CrossCore Embedded Studio, run the command: | ||
+ | * sudo dpkg -i adi-CrossCoreEmbeddedStudio-linux-x86-2.6.0.deb | ||
+ | |||
+ | The Ubuntu Linux Installer(Debian) installs all necessary components to the Analog Devices local directory structure which can be found below. | ||
+ | |||
+ | * CrossCore Embedded Studio installs to **/ | ||
+ | * Eclipse IDE installs to **/ | ||
+ | * GNU ARM Embedded Toolchain for Cortex-M installs to **/ | ||
+ | * OpenOCD installs to **/ | ||
+ | * CMSIS Pack files are installed to **/ | ||
+ | |||
+ | ====== Activating CrossCore Embedded Studio ====== | ||
+ | |||
+ | The first time you launch CrossCore Embedded Studio, you will be prompted to input a serial number, name, and email address. | ||
+ | |||
+ | Once the serial number has been activated, the CrossCore development tools will allow you full and unlimited access to all the features of the tool when using the Analog Devices family of ARM Cortex Processor. | ||
+ | |||
+ | ====== CrossCore Embedded Studio Support ====== | ||
+ | |||
+ | For more details on CrossCore Embedded Studio, updated versions of the tools, release notes, tools documentation, | ||
+ | |||
+ | //End of Document// | ||
+ | |||
+ | **[[resources: |