This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:eval:user-guides:eval-cog-ad3029lz:software:sensor [11 Aug 2017 08:20] – created Pranit Jadhav | resources:eval:user-guides:eval-cog-ad3029lz:software:sensor [11 Aug 2017 16:16] (current) – [Downloading the Sensor Software Pack] Pranit Jadhav | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Sensor Application Software Packs and Drivers ====== | ====== Sensor Application Software Packs and Drivers ====== | ||
===== General Description/ | ===== General Description/ | ||
- | Sensor software pack contains sensor software components. Sensor components are based on the sensor classes which abstract the functionality across sensor types. The Sensors software pack provides access to all the necessary add-on module digital drivers that attach to the [[ADI> | + | Sensor software pack contains sensor software components. Sensor components are based on the sensor classes which abstract the functionality across sensor types. The Sensors software pack provides access to all the necessary add-on module digital drivers that attach to the [[ADI> |
+ | |||
+ | ADI Sensor Software requires CrossCore Embedded Studio 2.6.0 ® , ADuCM3029 Device Family Pack 2.0.0 and EV-COG-AD3029LZ Board Support Package 1.0.0. | ||
- | ADI Sensor Software requires CrossCore Embedded Studio 2.6.0 ® , ADuCM302x Device Family Pack 2.0.0 and EV-COG-AD3029LZ Board Support Package 1.0.0. | + | The following application examples and sensor drivers are provided as part of the Sensor software pack: |
- | + | * Accelerometer | |
- | The following application examples and sensor drivers are provided as part of the Sensor software pack: | + | * Temperature Sensor |
- | + | * Visible Light Sensor | |
- | | + | |
- | * [[resources: | + | |
- | * [[resources: | + | |
- | + | ||
- | | + | |
For detailed information regarding the Sensor software pack, please see our complete Sensor software user guide. | For detailed information regarding the Sensor software pack, please see our complete Sensor software user guide. | ||
Line 28: | Line 25: | ||
===== Downloading the Sensor Software Pack ===== | ===== Downloading the Sensor Software Pack ===== | ||
- | The software pack can be downloaded in several | + | The software pack can be downloaded in following |
- Downloaded via the tools program | - Downloaded via the tools program | ||
* It is **recommended** to download the Sensor software pack through from the tools program you are using. | * It is **recommended** to download the Sensor software pack through from the tools program you are using. | ||
Line 39: | Line 36: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | Download the Sensor Software Pack to your computer. | + | Download the Sensor Software Pack. |
- | ADD LINK HERE SENSOR SOFTWARE PACK | + | [[http:// |
\\ | \\ |