This shows you the differences between two versions of the page.
Previous revisionNext revision | |||
— | resources:eval:user-guides:eval-cog-ad3029lz:software:connectivity [11 Aug 2017 12:18] – [Downloading the Sensor Software Pack] Pranit Jadhav | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== Connectivity Pack ====== | ||
+ | ===== General Description/ | ||
+ | Connectivity pack includes Bluetooth Low Energy (BLE) drivers for EV-COG-AD3029LZ. | ||
+ | Following are the requirements to use BLE drives available in the pack. | ||
+ | - [[resources: | ||
+ | - [[resources: | ||
+ | |||
+ | Connectivity Pack for BLE contains the following examples | ||
+ | - FindMe Target | ||
+ | - Proximity Reporter | ||
+ | - Data Exchange (Hello World) | ||
+ | |||
+ | ===== Downloading the Sensor Software Pack ===== | ||
+ | |||
+ | The software pack can be downloaded in following way. | ||
+ | - Downloaded via the tools program | ||
+ | * It is **recommended** to download the Connectivity software pack through from the tools program you are using. | ||
+ | \\ | ||
+ | |||
+ | <WRAP center round download 80%> | ||
+ | Download the Connectivity Software Pack to your computer. | ||
+ | |||
+ | ADD LINK HERE SENSOR SOFTWARE PACK | ||
+ | |||
+ | </ | ||
+ | |||
+ | \\ | ||