This version is outdated by a newer approved version.This version (31 Jul 2017 14:51) is a draft.
Approvals: 0/1
This is an old revision of the document!
ADuCM302x On-Chip Peripheral Drivers & Software
General Description/Overview
The ADuCM302x Device Family Pack (DFP) provides access to all the necessary on-chip peripheral drivers for both the ADuCM3029 and the ADuCM3027 devices. This software layer is the foundation layer needed when writing applications using this microprocessor family. When combined with the EV-COG-AD3029LZ software pack as well as the Sensors software pack, there are many great Internet of Things(IoT) applications and demos that can be replicated using the EV-COG-AD3029LZ development platform.
The following on-chip drivers are provided as part of the ADuCM302x Device Family Pack:
spi
i2c
uart
sport
beep
wdt
gpio
rtc
dma
cryto
adc
tmr
For detailed information regarding the ADuCM302x DFP, please see our complete ADuCM302x software user guide.
You MUST have this software package installed on your laptop or PC in order to compile, debug, and run the applications for the EV-COG-AD3029LZ platform.
Downloading the ADuCM302x Software Pack
The software pack can be installed directly by the tool chain's CMSIS pack manager. Optionally, you may download and then use the CMSIS pack manager's manual installation to install the pack.
Downloaded via the tool chain's CMSIS pack manager
It is
recommended to download the ADuCM302x software pack through from the tool chain's CMSIS pack manager. That way, all the files, directories structure, and project structure for the various applications is properly saved and accessed. For a detailed description on how to download the ADuCM302x software pack through CrossCore Embedded Studio please see our
CrossCore Embedded Studio Quickstart User Guide.
Downloaded to local directory
However if you do decide to download the ADuCM302x software pack to your PC/laptop directly, please use the link below to download the pack file from Keil's website. You will then need to “import” the pack file using your tool chain's CMSIS pack manager's import feature. Note that all software packs can be downloaded from Keil's website.
End of Document