This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:eval-cog-ad3029:software:aducm302x [31 Jul 2017 14:47] – Pranit Jadhav | resources:eval:user-guides:eval-cog-ad3029:software:aducm302x [31 Jul 2017 15:23] – Pranit Jadhav | ||
---|---|---|---|
Line 2: | Line 2: | ||
===== General Description/ | ===== General Description/ | ||
- | The ADuCM302x Device Family Pack (DFP) provides access to all the necessary on-chip peripheral drivers for both the [[ADI> | + | The ADuCM302x Device Family Pack (DFP) provides access to all the necessary on-chip peripheral drivers for both the [[ADI> |
The following on-chip drivers are provided as part of the ADuCM302x Device Family Pack: | The following on-chip drivers are provided as part of the ADuCM302x Device Family Pack: | ||
Line 27: | Line 27: | ||
<WRAP center round important 60%> | <WRAP center round important 60%> | ||
- | You **MUST** have this software package installed on your laptop or PC in order to compile, debug, and run the applications for the ADICUP3029 | + | You **MUST** have this software package installed on your laptop or PC in order to compile, debug, and run the applications for the EV-COG-AD3029LZ |
</ | </ |