This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adxl313z:no-os-setup [03 Jun 2022 11:47] – [Basic Project] George Mois | resources:eval:user-guides:eval-adxl313z:no-os-setup [03 Jun 2022 11:49] – [IIO Project] George Mois | ||
---|---|---|---|
Line 156: | Line 156: | ||
</ | </ | ||
- | When running make command make sure to specify the platform you want to build the project for. | + | When running make command make sure to specify the platform you want to build the project for. |
=== Project Description === | === Project Description === | ||
- | This project is actually a TINYIIOD demo for the used breakout board. The project launches a TINYIIOD server on the board so that the user may connect to it via an IIO client. Using IIO-Oscilloscope, | + | This project is actually a TINYIIOD demo for the used breakout board (the code is available [[repo> |
If you are not familiar with ADI IIO Application, | If you are not familiar with ADI IIO Application, |