This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adtf3175d-nxz:system_update [07 Feb 2023 19:50] – Added Full NVM Update Andre Straker-Payne | resources:eval:user-guides:eval-adtf3175d-nxz:system_update [26 Feb 2024 16:28] (current) – removed nvm update details. Andre Straker-Payne | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== System Update ====== | ====== System Update ====== | ||
- | This page covers the methods of updating the flash | + | This page covers the methods of updating the flash. |
===== Firmware Update ===== | ===== Firmware Update ===== | ||
+ | Firmware can be updated via the bin file. | ||
- | ===== Full Flash/NVM Update ===== | + | In general, the data_collect executable is used to update the firmware. This can be done from the host or on the device. |
- | The imager module includes a flash/NVM that contains all firmware | + | The firmware |
- | + | | |
- | Updating the full flash should only be done if absolutely needed. | + | |
- | + | ||
- | ==== Generating the Flash Image ==== | + | |
- | + | ||
- | + | ||
- | + | ||
- | ==== Programming the Flash ==== | + | |
- | + | ||
- | <note important> | + | |
- | + | ||
- | It is also possible to reprogram | + | |
- | + | ||
- | On the file system of the evaluation platform see the directory | + | |
- | + | ||
- | This procedure requires the ADSD3500 firmware streams, imager CFG and a CCB. | + | |
- | + | ||
- | While the CCB can be read via the ADSD3500, at this point the CFG cannot. This will be rectified in future versions of the ADSD3500 | + | |
- | + | ||
- | These operations are done entirely on the embedded Linux platform. | + | |
- | + | ||
- | The following steps are required: | + | |
- | | + | |
- | - Build the new NVM/flash image. | + | |
- | - Program the NVM/flash via Pulsatrix. | + | |
- | + | ||
- | === Read the CCB === | + | |
+ | From the host: | ||
< | < | ||
- | cd | + | cd " |
- | ./CCB my_ccb_file.ccb | + | data_collect --fw ..\image\NXP-Img-Rel4.1.1-ADTF3175D-0A8ED2B5\Fw_Update_4.1.5.bin --ip 10.42.0.1 tof-viewer_config.json |
</ | </ | ||
- | For example: | + | In either case wait for 60s before restarting |
- | + | ||
- | < | + | |
- | analog@aditof: | + | |
- | analog@aditof: | + | |
- | Done reading response header | + | |
- | Packets Needed: 86 | + | |
- | Packet number : 1 / 86 | + | |
- | Packet number : 2 / 86 | + | |
- | Packet number : 3 / 86 | + | |
- | Packet number : 4 / 86 | + | |
- | Packet number : 5 / 86 | + | |
- | Packet number : 6 / 86 | + | |
- | Packet number : 7 / 86 | + | |
- | Packet number : 8 / 86 | + | |
- | Packet number : 9 / 86 | + | |
- | Packet number : 10 / 86 | + | |
- | Packet number : 11 / 86 | + | |
- | Packet number : 12 / 86 | + | |
- | Packet number : 13 / 86 | + | |
- | Packet number : 14 / 86 | + | |
- | Packet number : 15 / 86 | + | |
- | Packet number : 16 / 86 | + | |
- | Packet number : 17 / 86 | + | |
- | Packet number : 18 / 86 | + | |
- | Packet number : 19 / 86 | + | |
- | Packet number : 20 / 86 | + | |
- | Packet number : 21 / 86 | + | |
- | Packet number : 22 / 86 | + | |
- | Packet number : 23 / 86 | + | |
- | Packet number : 24 / 86 | + | |
- | Packet number : 25 / 86 | + | |
- | Packet number : 26 / 86 | + | |
- | Packet number : 27 / 86 | + | |
- | Packet number : 28 / 86 | + | |
- | Packet number : 29 / 86 | + | |
- | Packet number : 30 / 86 | + | |
- | Packet number : 31 / 86 | + | |
- | Packet number : 32 / 86 | + | |
- | Packet number : 33 / 86 | + | |
- | Packet number : 34 / 86 | + | |
- | Packet number : 35 / 86 | + | |
- | Packet number : 36 / 86 | + | |
- | Packet number : 37 / 86 | + | |
- | Packet number : 38 / 86 | + | |
- | Packet number : 39 / 86 | + | |
- | Packet number : 40 / 86 | + | |
- | Packet number : 41 / 86 | + | |
- | Packet number : 42 / 86 | + | |
- | Packet number : 43 / 86 | + | |
- | Packet number : 44 / 86 | + | |
- | Packet number : 45 / 86 | + | |
- | Packet number : 46 / 86 | + | |
- | Packet number : 47 / 86 | + | |
- | Packet number : 48 / 86 | + | |
- | Packet number : 49 / 86 | + | |
- | Packet number : 50 / 86 | + | |
- | Packet number : 51 / 86 | + | |
- | Packet number : 52 / 86 | + | |
- | Packet number : 53 / 86 | + | |
- | Packet number : 54 / 86 | + | |
- | Packet number : 55 / 86 | + | |
- | Packet number : 56 / 86 | + | |
- | Packet number : 57 / 86 | + | |
- | Packet number : 58 / 86 | + | |
- | Packet number : 59 / 86 | + | |
- | Packet number : 60 / 86 | + | |
- | Packet number : 61 / 86 | + | |
- | Packet number : 62 / 86 | + | |
- | Packet number : 63 / 86 | + | |
- | Packet number : 64 / 86 | + | |
- | Packet number : 65 / 86 | + | |
- | Packet number : 66 / 86 | + | |
- | Packet number : 67 / 86 | + | |
- | Packet number : 68 / 86 | + | |
- | Packet number : 69 / 86 | + | |
- | Packet number : 70 / 86 | + | |
- | Packet number : 71 / 86 | + | |
- | Packet number : 72 / 86 | + | |
- | Packet number : 73 / 86 | + | |
- | Packet number : 74 / 86 | + | |
- | Packet number : 75 / 86 | + | |
- | Packet number : 76 / 86 | + | |
- | Packet number : 77 / 86 | + | |
- | Packet number : 78 / 86 | + | |
- | Packet number : 79 / 86 | + | |
- | Packet number : 80 / 86 | + | |
- | Packet number : 81 / 86 | + | |
- | Packet number : 82 / 86 | + | |
- | Packet number : 83 / 86 | + | |
- | Packet number : 84 / 86 | + | |
- | Packet number : 85 / 86 | + | |
- | Packet number : 86 / 86 | + | |
- | Binary size : 175148 | + | |
- | + | ||
- | CCB checksum correct! | + | |
- | analog@aditof: | + | |
- | -rw-rw-r-- 1 analog analog 175144 Feb 7 18:35 my_ccb_file.ccb | + | |
- | </ | + | |
- | + | ||
- | === Build the New NVM/Flash Image === | + | |
- | + | ||
- | < | + | |
- | ~/ | + | |
- | ./flash_gen -F -A -D ../ | + | |
- | </ | + | |
- | + | ||
- | For example: | + | |
- | < | + | |
- | analog@aditof: | + | |
- | sizeof(CCB) : 0x40000 | + | |
- | sizeof(INIT) : 0x3000 | + | |
- | sizeof(PF) : 0x20000 | + | |
- | sizeof(PC) : 0x20000 | + | |
- | sizeof(PU) : 0x20000 | + | |
- | sizeof(CDEBUG) : 0x4000 | + | |
- | sizeof(IMAGER) : 0x10000 | + | |
- | sizeof(CAP_CHUNK) : 0x1000 | + | |
- | FILE_HEADER | + | |
- | file_header.chunkHeaderCRC = 0xbb1bb508 | + | |
- | file_header.nextChunkHeader = 0x1000 | + | |
- | CAPABILITIES CHUNK | + | |
- | cap_t.header.nextChunkHeader = 0x2000 | + | |
- | cap_size = 40 | + | |
- | cap.header.chunkSizeBytes = 0x44 | + | |
- | cap_t.header.chunkHeaderCRC = 0xad6384e4 | + | |
- | cap_crc = 0x36362162 | + | |
- | D = ../ | + | |
- | optind=4 | + | |
- | ccb.header.nextChunkHeader = 270336 | + | |
- | ccb_size = 2ac28 | + | |
- | ccb.header.chunkSizeBytes = 2ac2c | + | |
- | ccb.header.chunkHeaderCRC = 0x2ef9475d | + | |
- | ccb_crc = 0x761ea8a5 | + | |
- | X = ./ | + | |
- | optind=6 | + | |
- | imager.header.nextChunkHeader = 0x52000 | + | |
- | imager_size = e772 | + | |
- | imager.header.chunkSizeBytes = e776 | + | |
- | imager.header.chunkHeaderCRC = 0xd954c29e | + | |
- | imager_crc = 0xd60bb444 | + | |
- | P = adsd3500_fw_3_2_2.stream | + | |
- | optind=8 | + | |
- | pf.header.nextChunkHeader = 72000 | + | |
- | pf_size = 167ac | + | |
- | pf.header.chunkSizeBytes = 167ac | + | |
- | Q = adsd3500_fw_3_2_2.stream | + | |
- | optind=10 | + | |
- | pc.header.nextChunkHeader = 92000 | + | |
- | pf_size = 167ac | + | |
- | pc.header.chunkSizeBytes = 167ac | + | |
- | R = adsd3500_fw_3_2_2.stream | + | |
- | optind=12 | + | |
- | pc.header.nextChunkHeader = b2000 | + | |
- | pf_size = 167ac | + | |
- | pu.header.chunkSizeBytes = 167ac | + | |
- | last_chunk = 1 | + | |
- | I = Init_firmware_apps_board_25MHZ.stream | + | |
- | optind=15 | + | |
- | init.header.nextChunkHeader = 0 | + | |
- | init_size = 208c | + | |
- | init.header.chunkSizeBytes = 2090 | + | |
- | init.header.chunkHeaderCRC = 0x7d0e005f | + | |
- | analog@aditof: | + | |
- | -rw-rw-r-- 1 analog analog 741376 Feb 7 18:41 flash.bin | + | |
- | </ | + | |
- | + | ||
- | === Program the NVM/flash via Pulsatrix === | + | |
- | < | + | |
- | cd ~/ | + | |
- | ./FW_UPDATE Flash_Binary_generator/ | + | |
- | </ | + | |
- | + | ||
- | When complete, let the system | + | |
- | + | ||
- | For example: | + | |
- | < | + | |
- | analog@aditof: | + | |
- | Size of Binary: 741376 | + | |
- | Packets Needed: 2896 | + | |
- | Actual size (after padding): 741376 | + | |
- | Computed CRC: 7629939a | + | |
- | Header data: ad00011200500b006e0000009a932976 | + | |
- | Packet number: 2896 / 2896 | + | |
- | Done | + | |
- | </ | + |