This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:eval:user-guides:eval-adtf3175d-nxz:system_update [02 Feb 2023 18:52] – created Andre Straker-Payne | resources:eval:user-guides:eval-adtf3175d-nxz:system_update [26 Feb 2024 16:28] (current) – removed nvm update details. Andre Straker-Payne | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== System Update ====== | ====== System Update ====== | ||
- | This page covers the methods of updating the flash | + | This page covers the methods of updating the flash. |
===== Firmware Update ===== | ===== Firmware Update ===== | ||
+ | Firmware can be updated via the bin file. | ||
- | ===== Full Flash/NVM Update ===== | + | In general, the data_collect executable is used to update the firmware. This can be done from the host or on the device. |
- | The imager module includes a flash/NVM that contains all firmware | + | The firmware |
- | + | * Fw_Update_4.1.5.bin | |
- | Updating the full flash should only be done if absolutely needed. | + | |
- | + | ||
- | ==== Generating | + | |
- | + | ||
- | ==== Programming | + | |
+ | From the host: | ||
+ | < | ||
+ | cd " | ||
+ | data_collect --fw ..\image\NXP-Img-Rel4.1.1-ADTF3175D-0A8ED2B5\Fw_Update_4.1.5.bin --ip 10.42.0.1 tof-viewer_config.json | ||
+ | </ | ||
+ | In either case wait for 60s before restarting the system. |