This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adtf3175d-nxz:system_update [07 Feb 2023 20:01] – [Firmware Update] Andre Straker-Payne | resources:eval:user-guides:eval-adtf3175d-nxz:system_update [10 Feb 2023 17:26] – Removed some unnecessary headings. Andre Straker-Payne | ||
---|---|---|---|
Line 14: | Line 14: | ||
On the device: | On the device: | ||
< | < | ||
- | cd Eval/bin | + | cd ~/Eval/bin |
./ | ./ | ||
</ | </ | ||
Line 20: | Line 20: | ||
From the host: | From the host: | ||
< | < | ||
- | C:\Analog Devices\ADTF3175D\TOF_Evaluation_ADTF3175D-Rel4.0.0\bin | + | cd "C:\Analog Devices\ADTF3175D\TOF_Evaluation_ADTF3175D-Rel4.0.0\bin" |
data_collect --fw Fw_Update_4.1.0.bin --ip 10.42.0.1 tof-viewer_config.json | data_collect --fw Fw_Update_4.1.0.bin --ip 10.42.0.1 tof-viewer_config.json | ||
</ | </ | ||
Line 28: | Line 28: | ||
Updating the full flash should only be done if absolutely needed. | Updating the full flash should only be done if absolutely needed. | ||
- | |||
- | ==== Generating the Flash Image ==== | ||
- | |||
- | |||
- | |||
- | ==== Programming the Flash ==== | ||
<note important> | <note important> |