This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:eval-adtf3175d-nxz:system_update [24 Nov 2023 14:49] – Remove on device update section. Andre Straker-Payne | resources:eval:user-guides:eval-adtf3175d-nxz:system_update [26 Feb 2024 16:28] (current) – removed nvm update details. Andre Straker-Payne | ||
---|---|---|---|
Line 19: | Line 19: | ||
In either case wait for 60s before restarting the system. | In either case wait for 60s before restarting the system. | ||
- | ===== Full Flash/NVM Update ===== | ||
- | |||
- | The imager module includes a flash/NVM that contains all firmware and calibration parameters for to enable the imager (ADSD3100 or ADSD3030) and the ADSD3500. | ||
- | |||
- | Updating the full flash should only be done if absolutely needed. | ||
- | |||
- | <note important> | ||
- | |||
- | It is also possible to reprogram the full NVM/flash of the module. | ||
- | |||
- | On the file system of the evaluation platform see the directory /// | ||
- | |||
- | This procedure requires the ADSD3500 firmware streams, imager CFG and a CCB. | ||
- | |||
- | While the CCB can be read via the ADSD3500, at this point the CFG cannot. This will be rectified in future versions of the ADSD3500 firmware. For now, ensure you have the correct CFG for ADI. | ||
- | |||
- | The firmware stream files for the latest version is available on the respective flash image. Stream files can be also obtained from the ADSD3500 installer. From the installer package, under the directory ADSD3500_Release_Firmware, | ||
- | * ADSD3500_Init_firmware_25MHz.stream | ||
- | * ADSD3500_Firmware_Host_Boot_4_1_0.stream | ||
- | |||
- | These operations are done entirely on the embedded Linux platform. | ||
- | |||
- | The following steps are required: | ||
- | - Read the CCB from the device. | ||
- | - Build the new NVM/flash image. | ||
- | - Program the NVM/flash via Pulsatrix. | ||
- | |||
- | === Read the CCB === | ||
- | |||
- | < | ||
- | cd ~/ | ||
- | ./CCB my_ccb_file.ccb | ||
- | </ | ||
- | |||
- | For example: | ||
- | |||
- | < | ||
- | analog@aditof: | ||
- | analog@aditof: | ||
- | Done reading response header | ||
- | Packets Needed: 86 | ||
- | Packet number : 1 / 86 | ||
- | Packet number : 2 / 86 | ||
- | Packet number : 3 / 86 | ||
- | Packet number : 4 / 86 | ||
- | Packet number : 5 / 86 | ||
- | Packet number : 6 / 86 | ||
- | Packet number : 7 / 86 | ||
- | Packet number : 8 / 86 | ||
- | Packet number : 9 / 86 | ||
- | Packet number : 10 / 86 | ||
- | Packet number : 11 / 86 | ||
- | Packet number : 12 / 86 | ||
- | Packet number : 13 / 86 | ||
- | Packet number : 14 / 86 | ||
- | Packet number : 15 / 86 | ||
- | Packet number : 16 / 86 | ||
- | Packet number : 17 / 86 | ||
- | Packet number : 18 / 86 | ||
- | Packet number : 19 / 86 | ||
- | Packet number : 20 / 86 | ||
- | Packet number : 21 / 86 | ||
- | Packet number : 22 / 86 | ||
- | Packet number : 23 / 86 | ||
- | Packet number : 24 / 86 | ||
- | Packet number : 25 / 86 | ||
- | Packet number : 26 / 86 | ||
- | Packet number : 27 / 86 | ||
- | Packet number : 28 / 86 | ||
- | Packet number : 29 / 86 | ||
- | Packet number : 30 / 86 | ||
- | Packet number : 31 / 86 | ||
- | Packet number : 32 / 86 | ||
- | Packet number : 33 / 86 | ||
- | Packet number : 34 / 86 | ||
- | Packet number : 35 / 86 | ||
- | Packet number : 36 / 86 | ||
- | Packet number : 37 / 86 | ||
- | Packet number : 38 / 86 | ||
- | Packet number : 39 / 86 | ||
- | Packet number : 40 / 86 | ||
- | Packet number : 41 / 86 | ||
- | Packet number : 42 / 86 | ||
- | Packet number : 43 / 86 | ||
- | Packet number : 44 / 86 | ||
- | Packet number : 45 / 86 | ||
- | Packet number : 46 / 86 | ||
- | Packet number : 47 / 86 | ||
- | Packet number : 48 / 86 | ||
- | Packet number : 49 / 86 | ||
- | Packet number : 50 / 86 | ||
- | Packet number : 51 / 86 | ||
- | Packet number : 52 / 86 | ||
- | Packet number : 53 / 86 | ||
- | Packet number : 54 / 86 | ||
- | Packet number : 55 / 86 | ||
- | Packet number : 56 / 86 | ||
- | Packet number : 57 / 86 | ||
- | Packet number : 58 / 86 | ||
- | Packet number : 59 / 86 | ||
- | Packet number : 60 / 86 | ||
- | Packet number : 61 / 86 | ||
- | Packet number : 62 / 86 | ||
- | Packet number : 63 / 86 | ||
- | Packet number : 64 / 86 | ||
- | Packet number : 65 / 86 | ||
- | Packet number : 66 / 86 | ||
- | Packet number : 67 / 86 | ||
- | Packet number : 68 / 86 | ||
- | Packet number : 69 / 86 | ||
- | Packet number : 70 / 86 | ||
- | Packet number : 71 / 86 | ||
- | Packet number : 72 / 86 | ||
- | Packet number : 73 / 86 | ||
- | Packet number : 74 / 86 | ||
- | Packet number : 75 / 86 | ||
- | Packet number : 76 / 86 | ||
- | Packet number : 77 / 86 | ||
- | Packet number : 78 / 86 | ||
- | Packet number : 79 / 86 | ||
- | Packet number : 80 / 86 | ||
- | Packet number : 81 / 86 | ||
- | Packet number : 82 / 86 | ||
- | Packet number : 83 / 86 | ||
- | Packet number : 84 / 86 | ||
- | Packet number : 85 / 86 | ||
- | Packet number : 86 / 86 | ||
- | Binary size : 175148 | ||
- | |||
- | CCB checksum correct! | ||
- | analog@aditof: | ||
- | -rw-rw-r-- 1 analog analog 175144 Feb 7 18:35 my_ccb_file.ccb | ||
- | </ | ||
- | |||
- | === Build the New NVM/Flash Image === | ||
- | |||
- | < | ||
- | ~/ | ||
- | ./flash_gen -F -A -D ../ | ||
- | </ | ||
- | |||
- | For example: | ||
- | < | ||
- | analog@aditof: | ||
- | sizeof(CCB) : 0x40000 | ||
- | sizeof(INIT) : 0x3000 | ||
- | sizeof(PF) : 0x20000 | ||
- | sizeof(PC) : 0x20000 | ||
- | sizeof(PU) : 0x20000 | ||
- | sizeof(CDEBUG) : 0x4000 | ||
- | sizeof(IMAGER) : 0x10000 | ||
- | sizeof(CAP_CHUNK) : 0x1000 | ||
- | FILE_HEADER | ||
- | file_header.chunkHeaderCRC = 0xbb1bb508 | ||
- | file_header.nextChunkHeader = 0x1000 | ||
- | CAPABILITIES CHUNK | ||
- | cap_t.header.nextChunkHeader = 0x2000 | ||
- | cap_size = 40 | ||
- | cap.header.chunkSizeBytes = 0x44 | ||
- | cap_t.header.chunkHeaderCRC = 0xad6384e4 | ||
- | cap_crc = 0x36362162 | ||
- | D = ../ | ||
- | optind=4 | ||
- | ccb.header.nextChunkHeader = 270336 | ||
- | ccb_size = 2ac28 | ||
- | ccb.header.chunkSizeBytes = 2ac2c | ||
- | ccb.header.chunkHeaderCRC = 0x2ef9475d | ||
- | ccb_crc = 0x761ea8a5 | ||
- | X = ./ | ||
- | optind=6 | ||
- | imager.header.nextChunkHeader = 0x52000 | ||
- | imager_size = e772 | ||
- | imager.header.chunkSizeBytes = e776 | ||
- | imager.header.chunkHeaderCRC = 0xd954c29e | ||
- | imager_crc = 0xd60bb444 | ||
- | P = adsd3500_fw_3_2_2.stream | ||
- | optind=8 | ||
- | pf.header.nextChunkHeader = 72000 | ||
- | pf_size = 167ac | ||
- | pf.header.chunkSizeBytes = 167ac | ||
- | Q = adsd3500_fw_3_2_2.stream | ||
- | optind=10 | ||
- | pc.header.nextChunkHeader = 92000 | ||
- | pf_size = 167ac | ||
- | pc.header.chunkSizeBytes = 167ac | ||
- | R = adsd3500_fw_3_2_2.stream | ||
- | optind=12 | ||
- | pc.header.nextChunkHeader = b2000 | ||
- | pf_size = 167ac | ||
- | pu.header.chunkSizeBytes = 167ac | ||
- | last_chunk = 1 | ||
- | I = Init_firmware_apps_board_25MHZ.stream | ||
- | optind=15 | ||
- | init.header.nextChunkHeader = 0 | ||
- | init_size = 208c | ||
- | init.header.chunkSizeBytes = 2090 | ||
- | init.header.chunkHeaderCRC = 0x7d0e005f | ||
- | analog@aditof: | ||
- | -rw-rw-r-- 1 analog analog 741376 Feb 7 18:41 flash.bin | ||
- | </ | ||
- | |||
- | === Program the NVM/flash via Pulsatrix === | ||
- | < | ||
- | cd ~/ | ||
- | ./FW_UPDATE Flash_Binary_generator/ | ||
- | </ | ||
- | |||
- | When complete, let the system perform the update for 1 minutes. From 4.2.0 of the ADSD3500 firmware, an indication of completion or failure will be available from the ADSD3500. | ||
- | |||
- | For example: | ||
- | < | ||
- | analog@aditof: | ||
- | Size of Binary: 741376 | ||
- | Packets Needed: 2896 | ||
- | Actual size (after padding): 741376 | ||
- | Computed CRC: 7629939a | ||
- | Header data: ad00011200500b006e0000009a932976 | ||
- | Packet number: 2896 / 2896 | ||
- | Done | ||
- | </ | ||
- | |||
- | Wait at least 30 seconds before restarting the system. |