This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adsd3100-nxz-gui [01 Aug 2021 11:08] – [EVAL_ADSD3100_NXZ Software Package] Harshvardhan Bhatia | resources:eval:user-guides:eval-adsd3100-nxz-gui [10 Apr 2024 18:26] (current) – More txt updates. Andre Straker-Payne | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== | + | ====== |
- | This user guide is to step through installation steps for the EVAL-ADSD3100-NXZ software package. | + | |
- | ==== Download Installer ==== | + | With Eval Kit software 5.0.0 there have been some major updates to ADIToFGUI, starting with the UX. |
- | * Download installer from here : | + | |
- | ==== Intro ==== | + | ===== Usage ===== |
- | * Once installer is downloaded, run the application to see this window. Click ' | + | |
- | {{ : | + | |
- | ==== License ==== | + | |
- | * Read through license and select 'I accept the agreement' | + | |
- | {{ : | + | |
- | ==== Installation Location ==== | + | |
- | * Select a location to install the package | + | |
- | * Click ' | + | |
- | {{ : | + | |
- | ==== GPU Capability ==== | + | |
- | * Select Yes to test GPU compatibility | + | |
- | * If GPU is compatible .... | + | |
- | ==== Done ==== | + | ==== Connecting |
- | * Once installation is done you can navigate to the installation folder to run the following applications: | + | |
- | * ADIToFGUI | + | |
- | * Data Collect | + | |
- | * Depth Compute | + | |
+ | 1. Open ADIToFGUI located in the installation " | ||
+ | {{: | ||
+ | 2. Select " | ||
+ | {{: | ||
+ | 3. Select the desired mode -> Play | ||
+ | {{: | ||
+ | |||
+ | 4. Streaming frames | ||
+ | |||
+ | {{: | ||
+ | |||
+ | ===== New Features ===== | ||
+ | |||
+ | ==== Adjusting the Ini Parameters ==== | ||
+ | |||
+ | It is now possible to adjust some of the configuration parameters during use. These parameters are generally stored in ini/JSON files are a per mode basis. The ADSD3500 and depth compute libraries receive the changed parameter values. | ||
+ | |||
+ | The **Ini Parameter** window can be selected at any point. Select **Ini Params** in the **Tools** menu.. To do so follow the image below. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | Once opened the **Ini Parameter** window can be use to adjust the parameter. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | **Modify** is needed to write the parameters to the device. Please note, the stream is stopped, the ADSD3500 and depth compute library updated, then the stream is restarted. | ||
+ | |||
+ | **Reset** is used to set the values in the ADSD3500 and depth compute library back to those from the original ini file. | ||
+ | |||
+ | **Save** saves the parameters listed in the window to the a file. | ||
+ | |||
+ | ===== Trouble Shooting ===== | ||
+ | |||
+ | ==== Slow Point Cloud Rendering ==== | ||
+ | |||
+ | If rendering of the point cloud is slow, it may be necessary to ensure the GPU is rendering and not the CPU. With an NVIDIA GPU you can do the following. | ||
+ | |||
+ | 1. NVIDIA Control Panel -> Manage 3D Settings -> Program Settings -> Add | ||
+ | |||
+ | {{: | ||
+ | |||
+ | 2. Browse | ||
+ | |||
+ | {{: | ||
+ | |||
+ | 3. Select the folder " | ||
+ | |||
+ | {{: | ||
+ | |||
+ | 4. For the select program " | ||
+ | |||
+ | {{: | ||
+ | |||
+ | |||
+ | |||
+ | |||
+ | |||
+ | ====== ADIToFGUI Eval Kit 4.3.0 or earlier ====== | ||
+ | This is a guide for the ToF module viewer. This page applies to the viewer for the following modules: | ||
+ | - [[: | ||
+ | - [[: | ||
+ | - [[: | ||
+ | |||
+ | ==== Start ==== | ||
+ | |||
+ | |||
+ | * Find the ADIToFGUI.exe in the ' | ||
+ | * v2.x.x | ||
+ | * Default location : C:\Analog Devices\TOF_Evaluation_BM-RelX.X.X\viewer\ | ||
+ | * v3.x.x | ||
+ | * Default location : C:\Analog Devices\TOF_Evaluation_BM-RelX.X.X\bin\ | ||
+ | * If you are evaluating the **EVAL-ADTF3175D-NXZ**: | ||
+ | * Confirm that an unidentified local network has been discovered by the pc - IP address = 10.42.0.1 | ||
+ | * Run TOF_Evaluation_BM-Relx.x.x | ||
+ | * Hit refresh until a Device is found | ||
+ | * **Select .json file based on your kits serial number** - Software Release version 4.2.0+ | ||
+ | * If your serial number starts with ' | ||
+ | * If your serial number starts with ' | ||
+ | * If you are evaluating the following modules : **EVAL-ADTF3175-NXZ** or **EVAL-ADSD3100-NXZ** (only supported with software release 2.1.1) | ||
+ | * Start the viewer to get to the window below | ||
+ | * If a camera is connected it should show up in the ' | ||
+ | * Select your device | ||
+ | * Select correct config file (depends on which module you are using) | ||
+ | * [[: | ||
+ | * [[: | ||
+ | * Click 'Open Device' | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ==== Run Camera ==== | ||
+ | * Once the device has been initialized the 'ToF Camera Options' | ||
+ | * Available modes will depend on the module serial number : [[: | ||
+ | * Select preferred view option (described below) and click play to run camera | ||
+ | |||
+ | {{: | ||
+ | |||
+ | <note important> | ||
+ | |||
+ | ==== Active Brightness and Depth ==== | ||
+ | * If this option is selected, the first window will show active brightness/ | ||
+ | * Depth is shown in mm, the user can hover over the image to see real-time depth data | ||
+ | {{ : | ||
+ | |||
+ | ==== Mode Switching ==== | ||
+ | * If the user wants to switch modes while the camera is running frames: | ||
+ | * Click ' | ||
+ | * Select mode in drop down menu | ||
+ | * Click ' | ||
+ | |||
+ | ==== Point Cloud and Depth ==== | ||
+ | * If camera is already running ' | ||
+ | * Click ' | ||
+ | * Select 'Point Cloud and Depth' | ||
+ | * Click ' | ||
+ | * If this option is selected, the first window will show a point-cloud generated from the depth on the second window. | ||
+ | * Point Cloud Controls: | ||
+ | * Zoom In/Out | ||
+ | * Use the mouse wheel and scroll forward to zoom in, scroll backwards to zoom out. | ||
+ | * Grab image and move it in all directions | ||
+ | * Hover over the Point Cloud Image and and drag the mouse while the right mouse button is pressed. Move slowly | ||
+ | * Rotate image | ||
+ | * Drage the mouse while pressing the left mouse button | ||
+ | * Increase / Decrease Point Cloud point size | ||
+ | * Grab the slider at the bottom of the Point Cloud window and move it left or right to decrease or increase the point size. | ||
+ | * Reset View | ||
+ | * Press the “Reset View” button to restore to default image size and position | ||
+ | {{: | ||
+ | |||
+ | ==== Recording ==== | ||
+ | * Recording via the GUI is deprecated, please use [[: | ||
+ | |||
+ | ===== Troubleshooting ===== | ||
+ | * Visit [[: |