This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adsd3100-nxz-gui [01 Aug 2021 11:08] – [EVAL_ADSD3100_NXZ Software Package] Harshvardhan Bhatia | resources:eval:user-guides:eval-adsd3100-nxz-gui [01 Aug 2021 11:46] – Initial Info Harshvardhan Bhatia | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== | + | ====== ADSD3100 |
- | This user guide is to step through installation steps for the EVAL-ADSD3100-NXZ software package. | + | This is a guide for the ToF viewer. |
- | ==== Download Installer ==== | ||
- | * Download installer from here : | ||
- | ==== Intro ==== | + | ==== Start ==== |
- | * Once installer is downloaded, run the application | + | * Start the viewer to get to the window |
- | {{ : | + | * If a camera is connected it should show up in the 'Open Device' |
- | ==== License ==== | + | * Select |
- | * Read through license and select 'I accept | + | |
- | {{ : | + | |
- | ==== Installation Location ==== | + | |
- | * Select | + | |
- | * Click ' | + | |
- | {{ : | + | |
- | ==== GPU Capability ==== | + | |
- | * Select Yes to test GPU compatibility | + | |
- | * If GPU is compatible .... | + | |
- | ==== Done ==== | + | {{ :resources: |
- | * Once installation is done you can navigate to the installation folder to run the following applications: | + | |
- | * ADIToFGUI | + | |
- | * Data Collect | + | |
- | * Depth Compute | + | |
+ | ==== Run Camera ==== | ||
+ | * Once the device has been initialized the 'ToF Camera Options' | ||
+ | * Available modes will depend on the module | ||
+ | * EVAL-ADSD-3100 : mp_pcm, qmp | ||
+ | * Select preferred view option (described below) and click play to run camera | ||
+ | {{ : | ||
+ | ==== Active Brightness and Depth ==== | ||
+ | * If this option is selected, the first window will show active brightness/ | ||
+ | * Depth is shown in mm, the user can hover over the image to see real-time depth data | ||
+ | ==== Point Cloud and Depth ==== | ||
+ | * If camera is already running ' | ||
+ | * Click ' | ||
+ | * Select 'Point Cloud and Depth' | ||
+ | * Click ' | ||
+ | * If this option is selected, the first window will show a point-cloud generated from the depth on the second window. | ||
+ | * The user can orient the point cloud by dragging the mouse while holding the right mouse button | ||
+ | * Click 'Reset View' in the point cloud window to reset the orientation. | ||
+ | |||
+ | {{ : | ||