This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:eval-adsd3100-nxz-gui [10 Apr 2024 18:23] – Added some text. Andre Straker-Payne | resources:eval:user-guides:eval-adsd3100-nxz-gui [10 Apr 2024 18:26] (current) – More txt updates. Andre Straker-Payne | ||
---|---|---|---|
Line 27: | Line 27: | ||
==== Adjusting the Ini Parameters ==== | ==== Adjusting the Ini Parameters ==== | ||
- | It is now possible to adjust some of the parameters | + | It is now possible to adjust some of the configuration |
- | The Ini Parameter window can be selected at any point. To do so follow the image below: | + | The **Ini Parameter** window can be selected at any point. Select **Ini Params** in the **Tools** menu.. To do so follow the image below. |
{{: | {{: | ||
- | Once opened the Ini Parameter window can be use to adjust the parameter. | + | Once opened the **Ini Parameter** window can be use to adjust the parameter. |
{{: | {{: |