This is an old revision of the document!
The Moduware platform allow users, hobbyists & makers to realize their ideas centered around IoT applications. The Moduware Developer’s Kit (MDK) essentially consists of
The development module (ADPAQ) is based on the [[adi>ADuCM3029] microcontroller. Various types of sensors/actuators can be interfaced with this module. The development module is connected to the Moduware gateway using the SPI interface. The Gateway collects the data from the development module and communicates the data to the mobile application via Bluetooth Low Energy (BLE) interface. The mobile application can send commands to get data from sensors connected to the development module or send actuation commands to the actuators.