Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:eval-adl5902-ardz [06 Sep 2019 03:56] Jhake Zebedee Aquinoresources:eval:user-guides:eval-adl5902-ardz [14 Jan 2021 05:24] (current) – use ez> / interwiki links Robin Getz
Line 2: Line 2:
 {{ :resources:eval:user-guides:ADL5902-top-clean.jpg?600 |EVAL-ADL5902-ARDZ}} {{ :resources:eval:user-guides:ADL5902-top-clean.jpg?600 |EVAL-ADL5902-ARDZ}}
  
-The **[[https://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-ADL5902-ARDZ.html#eb-overview|EVAL-ADL5902-ARDZ]]** shield illustrates the functionality of the **[[http://www.analog.com/en/products/rf-microwave/rf-power-detectors/rms-responding-power-detectors/adl5902.html|ADL5902]], a 50 MHz to 9 GHz 65 dB TruPwr™ RMS responding RF power detector**. The voltage outputs of the ADL5902 are routed to the **ANALOG IN** connector of the Arduino base board. This allows the RF power detector’s output voltage to be easily digitized and processed by the Arduino base board’s integrated six-channel ADC. The output of the ADL5902’s on-board temperature sensor is also routed to one of the ANALOG IN pins. +The **[[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-ADL5902-ARDZ.html#eb-overview|EVAL-ADL5902-ARDZ]]** shield illustrates the functionality of the **[[adi>en/products/rf-microwave/rf-power-detectors/rms-responding-power-detectors/adl5902.html|ADL5902]], a 50 MHz to 9 GHz 65 dB TruPwr™ RMS responding RF power detector**. The voltage outputs of the ADL5902 are routed to the **ANALOG IN** connector of the Arduino base board. This allows the RF power detector’s output voltage to be easily digitized and processed by the Arduino base board’s integrated six-channel ADC. The output of the ADL5902’s on-board temperature sensor is also routed to one of the ANALOG IN pins. 
  
 The **power supply** for the board comes from the Arduino base board through the POWER connector (5V). So while there is **no need to connect an external power supply**, the board can be powered by an external supply (6 Volt wall wart on **P3** or 6V connected to the **P1** screw terminals. The **power supply** for the board comes from the Arduino base board through the POWER connector (5V). So while there is **no need to connect an external power supply**, the board can be powered by an external supply (6 Volt wall wart on **P3** or 6V connected to the **P1** screw terminals.
  
-The EVAL-ADL5902-ARDZ is compatible with **EVAL-ADICUP3029** and **DC2026C**(also called **Linduino One**). For both platforms, **PC software GUI applications** ([[#Software GUI for EVAL-ADICUP3029|EVAL-ADICUP3029]], [[#Software GUI for Linduino|Linduino]]) are available using which, the user can make RF power measurements and also calibrate the device to decrease measurement error. **Device drivers** for [[#Development on EVAL-ADICUP3029|EVAL-ADICUP3029]] and for [[#Development on Linduino|Linduino Uno]] are also available, which the user may use to **develop their own code for RF measurement**, device calibration, and more.+The EVAL-ADL5902-ARDZ is designed to work as a shield for **EVAL-ADICUP3029** and **DC2026C**(also called **Linduino One**). For **EVAL-ADICUP3029** **PC software GUI application** ([[#Software GUI for EVAL-ADICUP3029|EVAL-ADICUP3029]]) is available. Using this, the user can make RF power measurements and also calibrate the device to decrease measurement error. **Device development drivers** for [[#Development on EVAL-ADICUP3029|EVAL-ADICUP3029]] are also available, which the user may use to **develop their own code** for RF measurement, device calibration, and more.
  
 ====== Shield Specifications ====== ====== Shield Specifications ======
Line 56: Line 56:
 ====== Software GUI for EVAL-ADICUP3029  ====== ====== Software GUI for EVAL-ADICUP3029  ======
 ===== Software Installation ===== ===== Software Installation =====
-  - Set up **EVAL-ADICUP3029 serial driver** as in **[[https://wiki.analog.com/resources/eval/user-guides/EVAL-ADICUP3029/tools/keil_iar_support#how_to_use_EVAL-ADICUP3029_with_iar|1. Install mBed windows serial driver...]]** +  - Set up **EVAL-ADICUP3029 serial driver** as in **[[/resources/eval/user-guides/EVAL-ADICUP3029/tools/keil_iar_support#how_to_use_EVAL-ADICUP3029_with_iar|1. Install mBed windows serial driver...]]** 
-  - Contact us at  [[https://ez.analog.com/rf/f/q-a|EngineeringZone]] to get the **Software GUI file** +  - Download the software on the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/eval-ad8302-ardz.html#|product page]]  or click [[adi>media/en/evaluation-boards-kits/evaluation-software/eval-ad8302-ardz%20evaluation%20software.zip|here]]. 
-  - Extract the Software GUI file to your computer.+  - Extract the Software GUI.zip to your computer.
   - Connect the EVAL-ADICUP3029 board using micro USB cable.   - Connect the EVAL-ADICUP3029 board using micro USB cable.
   - Set the **S2 switch to USB**.\\ {{:resources:eval:user-guides:rfdet-adicup3029-usb.png|EVAL-ADICUP3029pic_selectUSB}}   - Set the **S2 switch to USB**.\\ {{:resources:eval:user-guides:rfdet-adicup3029-usb.png|EVAL-ADICUP3029pic_selectUSB}}
Line 76: Line 76:
 ==== Measurement Window ==== ==== Measurement Window ====
  {{:resources:eval:user-guides:eval-adl5902-ardz-measurement.png|APP_window}}\\   {{:resources:eval:user-guides:eval-adl5902-ardz-measurement.png|APP_window}}\\ 
-The EVAL-ADL5902-ARDZ shield converts the measured ADC code to RF input power in dBm using stored calibration coefficients.  A 3-point calibration methodology is used. The software program includes default calibration coefficients that correspond to the default response of the ADL5902 across RF power level and frequency.  [[http://www.analog.com/media/en/technical-documentation/data-sheets/ADL5902.pdf|datasheet specifications of ADL5902]]. Because of part-to-part device variation, observed accuracy using the default calibration coefficients will be sub-optimal. By availing of the software program's 3-point calibration function, measurement accuracy can be increased.\\  +The EVAL-ADL5902-ARDZ shield converts the measured ADC code to RF input power in dBm using stored calibration coefficients.  A 3-point calibration methodology is used. The software program includes default calibration coefficients that correspond to the default response of the ADL5902 across RF power level and frequency.  [[adi>media/en/technical-documentation/data-sheets/ADL5902.pdf|datasheet specifications of ADL5902]]. Because of part-to-part device variation, observed accuracy using the default calibration coefficients will be sub-optimal. By availing of the software program's 3-point calibration function, measurement accuracy can be increased.\\  
 <WRAP><note>If calibration is skipped at some frequencies, the default calibration coefficients will be used (user calibration coefficients and default calibration coefficients are INITIALLY the same). </note></WRAP> \\  <WRAP><note>If calibration is skipped at some frequencies, the default calibration coefficients will be used (user calibration coefficients and default calibration coefficients are INITIALLY the same). </note></WRAP> \\ 
 Related topic: [[#Calibration Window|Calibration of EVAL-ADL5902-ARDZ]] Related topic: [[#Calibration Window|Calibration of EVAL-ADL5902-ARDZ]]
Line 170: Line 170:
 ===== C Development Guide ===== ===== C Development Guide =====
 ==== Installations ====   ==== Installations ====  
-  - Download and install **[[http://www.analog.com/en/design-center/processors-and-dsp/evaluation-and-development-software/adswt-cces.html#relatedsoftware| CrossCore Embedded Studio (CCES) 2.8.1]]**+  - Download and install **[[adi>en/design-center/processors-and-dsp/evaluation-and-development-software/adswt-cces.html#relatedsoftware| CrossCore Embedded Studio (CCES) 2.8.1]]**
   - Download and install **[[https://developer.mbed.org/handbook/Windows-serial-configuration|mBed windows serial driver]]**   - Download and install **[[https://developer.mbed.org/handbook/Windows-serial-configuration|mBed windows serial driver]]**
 <note>Assumes a fresh installation of all required software</note> <note>Assumes a fresh installation of all required software</note>
 ==== Setting Up CrossCore Embedded Studio ==== ==== Setting Up CrossCore Embedded Studio ====
-  - Install the following packs by following the **[[https://wiki.analog.com/resources/eval/user-guides/EVAL-ADICUP3029/tools/cces_user_guide#how_to_install_or_upgrade_packs_for_cces|How to install or upgrade Packs for CCES]]** guide:+  - Install the following packs by following the **[[/resources/eval/user-guides/EVAL-ADICUP3029/tools/cces_user_guide#how_to_install_or_upgrade_packs_for_cces|How to install or upgrade Packs for CCES]]** guide:
     * **ARM.CMSIS.5.4.0**     * **ARM.CMSIS.5.4.0**
     * **AnalogDevices.ADuCM302x_DFP.3.1.2**     * **AnalogDevices.ADuCM302x_DFP.3.1.2**
Line 196: Line 196:
   - Run installer as Administrator. During installation, **check "Add Python 3.7 to PATH" before clicking "Install Now"**\\ {{:resources:eval:user-guides:rfdet-py-path.png|rfdet-py-path}}   - Run installer as Administrator. During installation, **check "Add Python 3.7 to PATH" before clicking "Install Now"**\\ {{:resources:eval:user-guides:rfdet-py-path.png|rfdet-py-path}}
   - Install **pyserial**. For windows, enter **pip3.7 install pyserial** on command prompt.   - Install **pyserial**. For windows, enter **pip3.7 install pyserial** on command prompt.
-  - Download and install **[[https://www.jetbrains.com/pycharm/download/#section=windows|PyCharm]] community version**+  - Download and install any python IDE (eg. **[[https://www.jetbrains.com/pycharm/download/#section=windows|PyCharm]] community version**)
   - Download and install **[[https://developer.mbed.org/handbook/Windows-serial-configuration|mBed windows serial driver]]**   - Download and install **[[https://developer.mbed.org/handbook/Windows-serial-configuration|mBed windows serial driver]]**
  
-==== Setting Up PyCharm ====+==== Setting Up Python Development Library ====
   - Download **{{:resources:eval:user-guides:power_detector_python_code_example.zip|power_detector_python_code_example.zip}}** and unzip.   - Download **{{:resources:eval:user-guides:power_detector_python_code_example.zip|power_detector_python_code_example.zip}}** and unzip.
   - Install **Power Detector Python Code Example.exe**, the destination folder used is the “Scripts” directory where the python3.7 is located. For windows, the location path is similar to **C:\Users\MyUsername\AppData\Local\Programs\Python\Python37\Scripts**\\ {{:resources:eval:user-guides:rfdet-py-scripts.png|rfdet-py-scripts}}   - Install **Power Detector Python Code Example.exe**, the destination folder used is the “Scripts” directory where the python3.7 is located. For windows, the location path is similar to **C:\Users\MyUsername\AppData\Local\Programs\Python\Python37\Scripts**\\ {{:resources:eval:user-guides:rfdet-py-scripts.png|rfdet-py-scripts}}
-  - Launch PyCharm and set up PyCharm interpreter by clicking file>>settings>>Project>>Project Interpreter choose python 3.7 then click “Ok”.+  - Launch Python IDE and make sure to chose the python 3.7 as the interpreter.
  
-==== Development on PyCharm ====+==== Running Python Development Example Code====
   - Connect the EVAL-ADICUP3029 board using micro USB cable.   - Connect the EVAL-ADICUP3029 board using micro USB cable.
   - In the EVAL-ADICUP3029, set the S2 switch to USB.   - In the EVAL-ADICUP3029, set the S2 switch to USB.
-  - Download **[[http://www.analog.com/en/products/adl5902.html#product-evaluationkit|power_detector-firmware.hex]]**, then copy it to the DAPLINK directory. Wait for the window to exit automatically. Else, repeat the [[#Development on PyCharm|Development on PyCharm]] guide.+  - Unzip **power detector development code-release.zip** from **[[adi>media/en/evaluation-boards-kits/evaluation-software/eval-ad8302-ardz%20evaluation%20software.zip|evaluation software]]** 
 +  - Find and copy **power_detector-firmware.hex** to the DAPLINK directory. Wait for the window to exit automatically.
   - Press S1 (reset) button on the EVAL-ADICUP3029 and mount the EVAL-ADL5902-ARDZ to the EVAL-ADICUP3029   - Press S1 (reset) button on the EVAL-ADICUP3029 and mount the EVAL-ADL5902-ARDZ to the EVAL-ADICUP3029
-  - On PyCharm, go to File>>Open and browse for the **[[https://wiki.analog.com/_detail/resources/eval/user-guides/rfdet-py-example-code.png?id=resources%3Aeval%3Auser-guides%3Aeval-adl5902-ardz|\PycharmProjects\example code]]** directory. +  - On Python IDE, go to File>>Open and browse for the **[[#rfdet-py-example-code|\example code]]** directory. 
   - Click Project Tab located at left side of IDE and go to **adl5902** folder and double click **adl5902-getShieldReadings.py**   - Click Project Tab located at left side of IDE and go to **adl5902** folder and double click **adl5902-getShieldReadings.py**
   - Change the default Port number (“COM10”) in the example code. On your computer go to Control Panel>>Device Manager look for Ports (COM & LPT) find the port number of “mbed Serial Port”.   - Change the default Port number (“COM10”) in the example code. On your computer go to Control Panel>>Device Manager look for Ports (COM & LPT) find the port number of “mbed Serial Port”.
Line 224: Line 225:
 </WRAP> </WRAP>
 ====== Help and Support ====== ====== Help and Support ======
-For any queries regarding the hardware and evaluation software, contact us at **[[https://ez.analog.com/rf|EngineerZone]]**.+For any queries regarding the hardware and evaluation software, contact us at **[[ez>rf|EngineerZone]]**.
resources/eval/user-guides/eval-adl5902-ardz.txt · Last modified: 14 Jan 2021 05:24 by Robin Getz