This is an old revision of the document!
CrossCore Embedded Studio Quickstart User Guide
This page describes how to use the ADuCM36x Device Family Pack (DFP) with CrossCore Embedded Studio (CCES) to create, import, build and debug applications for the ADuCM360 processor. The ADuCM360 processor integrates an ARM Cortex-M3 microcontroller with dual 24-bit sigma delta analog to digital converters along with various other on-chip analog and digital blocks within a single package.
This page describes how to install and work with the Analog Devices ADuCM36x DFP to start developing applications for the EVAL-ADICUP360. This page also highlights common problems and how to avoid them.
Additional help documentation can be found by opening CCES and selecting “Help Contents” from the CCES Help menu.
This page covers:
How to install or upgrade the ADuCM36x Device Family Pack (DFP) an ARM CMSIS Pack for CCES
How to create a new project for the ADuCM360
How to add startup code and core components to a new project for the ADuCM360
How to import existing projects into your workspace
How to build projects for programming the ADuCM360
How to configure the Tools Settings used by an ADuCM360 project
How to configure the debug session for an ADuCM360 application
How to start and stop debugging an ADuCM360 application
How to create a Binary (.bin) or Intel Hex (.hex) file from an ADuCM360 application
How to debug an programs using an ADuCM362 and ADuCM363 Evaluation Board
We have a playlist of YOU TUBE VIDEOS that can help you understand different aspects of CrossCore Embedded Studio. The videos talk about the ADICUP3029, but the tools information is relevant for the ADICUP360 as well. CrossCore Embedded Studio Videos
Workspace and Projects
A CCES workspace is a folder (e.g. c:\Users\anon\cces\2.7.0) that contains project resources and metadata.
When projects are created or imported, details about that project are stored in the workspace. The workspace metadata also includes preferences set through the CCES Preferences dialog box and IDE window layouts.
By default, CCES creates new projects within your workspace folder.
Each time you start CCES, you will be prompted for a workspace location. You can opt to default to a workspace directory by choosing to use a workspace directory as your default. You will not be prompted the next time you open CCES.
How to install or upgrade the ADuCM36x Device Family Pack (DFP) or ARM CMSIS Pack for CCES
CCES 2.7.0 does not comes with the ADuCM36x Device Family Pack (DFP) or the ARM CMSIS Pack file pre-installed.
Installing the ADuCM36x DFP
Switch to the CMSIS Pack Manager perspective by selecting Window | Perspective | Open Perspective | Other… | CMSIS Pack Manager.
Once opened, select Check for Updates on Web ( blue arrows on the toolbar ). This may take a minute or two.
Choose Analog Devices and ADuCM360 Series in the Devices View.
Select the ADuCM36x CMSIS Pack version (choose version 1.0.2 or higher) from the Packs View.
Click the Install Action.
Installing the ARM CMSIS Pack
Switch to the CMSIS Pack Manager perspective by selecting Window | Perspective | Open Perspective | Other… | CMSIS Pack Manager.
Once opened, select Check for Updates on Web ( blue arrows on the toolbar ), if you have not already done so.
Choose ARM in the Devices View.
Select the
Generic and
ARM.CMSIS from the Packs View, and select the current version (
e.g. 5.1.0)
Click the Install Action.
Installing Locally Saved ADuCM36x Pack
Alternatively, the ADuCM36x Device Family Pack (DFP) files can be installed using a local downloaded copy.
After downloading the .pack files from the Keil website (https://www.keil.com/dd2/pack/), select the Import Packs button in the CMSIS Pack Manager's Packs View, choose the .pack file as shown in the screenshot below, and click Open.
You will be prompted to accept a license agreement and, after agreeing to it, the CMSIS-Pack file will be installed into CrossCore Embedded Studio's CMSIS-Pack installation directory (e.g. C:\Analog Devices\CrossCore Embedded Studio 2.7.0\ARM\packs\AnalogDevices).
How to create a new project for the ADuCM360
A project for ADuCM360 can be created using the New CrossCore Project Wizard. This wizard will guide you through the steps to create a new project.
To create a new project, go to the menu bar and find File → New → CrossCore Project.
Name the project, and then hit the Next button.
Choose Processor family ARM and select Processor type ADuCM360.
There is no Silicon Revision Option for the ADuCM360, so it defaults to “none”
Project configuration allows you to add additional Add-ins to your project, such as Pin Multiplexing and changing the template language for a generated main function etc. Typically no configuration or add-ons are necessary.
Finally, press Finish and the project will be created and you can begin writing your program.
How to add startup code and core components to a new project for the ADuCM360
A new or empty ADuCM360 project does not have startup code or a linker description file that maps code and data. It is necessary to add these components using the Run-time Environment (RTE) Configuration Editor.
CrossCore Projects created for Analog Devices' Cortex-M based processors, such as ADuCM360 include a system.rteconfig file. Opening this file within the IDE will open the RTE Configuration Editor. Components from the CMSIS-Pack, such as drivers and services, can be added to a project by selecting them in the editor and clicking Save.
At minimum, a new ADuCM360 project requires the Device::Startup, CMSIS::Core and Device::Global Configuration components to be added to the project.
Double-click on the system.rteconfig to open the RTE Configuration Editor.
Select Device::Startup, CMSIS::Core and Device::Global Configuration.
Click Save (Ctrl+S)
You can also choose Device::Startup and click the Resolve button to add dependant components
How to import existing projects into your workspace
There are three(3) methods for importing existing projects:
Examples that you have saved to a local drive on your PC.
Examples that come with the ADuCM36x Device Family Pack (DFP).
Examples which are in the ADICUP360 GIT repository (most up to date content).
How to Import Existing Projects Saved to a Local Drive
Select File | Import… from the CCES menu.
A dialog will pop-up with several importing options, choose the General | Existing Projects into Workspace option, and click Next
Select Browse in the dialog window and search for the saved project which is on your local drive.
(Optional) If the Copy projects into workspace option is checked, the project will be copied to your workspace folder and the newly copied project will be opened and used. This preserves the original version of the project.
Click Finish
How to Import Examples that come with the ADuCM36x Device Family Pack (DFP)
Opening CCES Examples using the CMSIS Pack Manager Perspective
Open CMSIS Pack Manager perspective by clicking “Open Perspective” icon on tool bar and selecting “CMSIS Pack Manager” in the Open Perspective window (or choose CMSIS Pack Manager perspective if already open).
From the Examples View, select the example that you would like to open.
Click the Copy Action button.
A dialog will pop-up showing the location where the example will be copied to. Click Copy to copy and open the example project.
Opening Examples using the CCES Example Browser
Launch the CCES Example Broswer by clicking on Help --> Browse Examples.
Select ADuCM36x_DFP[x.y.z] in Product drop-down list, select the example and click Open example. Then the example will be copied to your workspace.
How to Import Existing Projects from the GIT Repository
Open the GIT perspective by clicking “Open Perspective” icon on tool bar and selecting “Git” in the Open Perspective window (or choose the GIT perspective if already open).
Clone the Git repository which contains all the latest code and projects associated with the ADuCM360. Populate the
URI field with the following address.
-
Click Next, Next and then Finish. There may be a pause while the branches are fetched.
In the Git Repositories window, Right Click on the Projects folder and select Import Projects…
Select Import existing Eclipse projects
Click Next and then Finish
Select the project in the Project Explorer View.
Select the Cog icon from the View's toolbar.
After configuring your project, click Apply and/or OK.
Disabling/Enabling Semihosting
To enable/disable semi-hosting in your program, visit your project Tools Settings.
Change the semi-hosting support option under Linker | Libraries:
After configuring your project, click Apply and/or OK.
Right click on the project and select the Build Project.
How to build projects for programming the ADuCM360
Open the C perspective by clicking “Open Perspective” icon on tool bar and selecting C in the Open Perspective window (or choose the C perspective if already open).
Right click on the project and select the Build Project.
You will need to create a launch configuration to debug your ADuCM3029 program.
If you have already built a project, select that project in the Project Explorer View.
Right-click on the project and choose
Debug As and
Application with GDB and OpenOCD (Emulator)
In the Target tab, choose Target (processor) and in the drop-down select Analog Devices ADuCM360
In the Target tab, choose Interface and in the drop-down select ARM CMSIS-DAP compliant adapter
In the Main tab, ensure that your project is selected in the Project entry box.
If the correct project is not populated, click the
Browse… button and choose the project. Note that this is optional and you only need to choose a project if you want the
IDE to search a project for the built binaries (programs), otherwise you can leave this entry blank.
In the Main tab, ensure your binary (program) is selected in the Application entry box.
If the correct binary (program) is not populated, click on Search Project… and choose the binary (program) from those available in the chosen project.
If your binary (program) is not populated and it was not built from a project in your workspace (
i.e. you have a pre-built binary), then click the
Browse… button and search for your pre-built binary (program). Click
Open when you have found and selected the pre-built binary (program).
In the Common tab, you can add the debug configuration to your menu bar shortcuts, for both Debug mode or Run mode by simply ticking the checkboxes.
How to start and stop debugging an ADuCM360 application
Ensure that you have connected your EVAL-ADICUP360 board to your computer via the
DEBUG USB port (
P14 - the micro
USB connected closest to the DC barrel jack).
If you are already in the Debug Configurations dialog, then click Debug.
If you are in the C Perspective, then you can launch the last Debug session by clicking the Beetle Debug button on the toolbar.
You will be prompted to switch perspective to the Debug perspective. Click Yes. You can opt to not show this dialog again.
If your binary (program) was built with semi-hosting enabled, then CCES will warn you that you need to re-build the program when you want to run the program without a debugger attached.
If everything goes fine, in the Console window, you will see a report without errors.
As a reference, the full text should be similar to:
Open On-Chip Debugger (OpenOCD) 0.9.0
Licensed under GNU GPL v2
Report bugs to <openocd-devel@lists.sourceforge.net>
0
Info : select transport "swd"
adapter speed: 1000 kHz
cortex_m reset_config sysresetreq
Info : CMSIS-DAP: SWD Supported
Info : CMSIS-DAP: Interface Initialised (SWD)
Info : CMSIS-DAP: FW Version = 1.0
Info : SWCLK/TCK = 0 SWDIO/TMS = 1 TDI = 0 TDO = 0 nTRST = 0 nRESET = 1
Info : CMSIS-DAP: Interface ready
Info : clock speed 1000 kHz
Info : SWD IDCODE 0x2ba01477
Info : aducm360.cpu: hardware has 2 breakpoints, 1 watchpoints
Info : CHIPID 0x0284
memory bus access delay set to 6 tck
adapter speed: 1000 kHz
Info : accepting 'gdb' connection on tcp/3333
Your program's execution is stopped automatically at the first breakpoint which is at the beginning of main() loop. You can use the debug functions and features of the CCES environment. (Such as stepping through, breakpoints, register reads, variable values, etc.)
To terminate a debug session, click on the red Stop button on the toolbar.
Windows Firewall Access
If this is the first time you have launched OpenOCD, the Windows Firewall may pop-up a window asking for access. Click on “
Allow Access”.
Linux USB Access
When installing CCES for the first time, you'll be prompted to set up you system, so that you can access
USB without root access. If you need to set up access to your
USB after installation, perhaps because you answered no during the installation, then you can run the script in
opt/analog/cces/2.7.0/Setup/setup_openocd_permissions.sh with sudo access.
How to create a Binary (.bin) or Intel Hex (.hex) file for an ADuCM360 application
Starting with CrossCore Embedded Studio (CCES) 2.8.0, the Artifact of your project build can now be a Binary or Intel Hex file.
Ensure that your program is built with semi-hosting disabled by visiting Tools Settings | Linker | Libraries and change Semihosting support to nosys.specs or None, depending on your application set-up.
Rebuild your application.
Convert your application into Binary (.bin) or Intel Hex (.hex) format by visiting Tools Settings once more.
Select the Build Artifact tab.
Select Binary (or Intel Hex) as the Artifact Type.
Apply and Close
Rebuild your application.
How to debug programs using ADuCM362 and ADuCM363 Evaluation Boards
The ADuCM362/ADuCM363 evaluation board comes with an Segger J-Link OB emulator which is not supported out of the box by CrossCore Embedded Studio (CCES). However, using Segger's JLinkGDBServer, we can still create and debug our ADuCM362/3 projects using CCES. The following are instructions on how to set up your Debug configuration.
-
Run JLinkGDBServer:
In the JLinkGDBServer application, choose your Target device. For example, ADuCM362
.
Click OK to run the JLinkGDBServer.
Next create a CCES Debug configuration for your ADuCM362 project/program:
In the Target tab:
Change the command from
openocd
to the path to PackChk (
e.g. C:\analog\cces\2.8.1\ARM\packs\ARM\CMSIS\5.3.0\CMSIS\Utilities\Win32\PackChk.exe
) or another executable that will run.
We specify a different executable because running OpenOCD will fail and it will cause the launch configuration to terminate.
It is not necessary to set your target to be Analog Devices ADuCM36x
or your interface to Segger J-Link
but it may help you when identifying your Debug configuration later on.
In the Main tab:
In the Debugger tab:
In the Startup tab:
Add the following to Initialization commands:
monitor flash device = ADuCM362
monitor flash download=1
monitor flash breakpoints = 1
monitor clrbp
monitor endian little
monitor reset
monitor halt
monitor sleep 10
monitor speed auto
Add the following to Run commands:
monitor reg r13 = (0x00000000)
monitor reg pc = (0x00000004)
break main
continue
Click Debug to start loading and running your program.
End of Document