This is an old revision of the document!
The EVAL-CN0409-ARDZ shield is a low to high level water turbidity measurement system in combination with the EVAL-ADICUP360. It uses the ADPD105's ambient light rejection feature to make it ideal for applications where accurate, robust and non-contact turbidity measurements are critical.
When the project is being run for the first time a calibration procedure is required in order to achieve high accuracy results. The user must follow the steps described in the UART terminal when the application is started.
The user has the option to modify the solutions that are used for calibrating the device. Any values can be used for the points that are used for calibration, but a proper distribution along the 0 - 1000 NTU range must be taken into account.
These values can be edited in CN0409.h file inside the include folder within the project structure.
After the calibration sequence is done at least once, the calibration coefficients are saved in the controller flash memory and will be used the next time when a calibration is not done. The calibration can be repeated as desired. If the program is run for the first time and a calibration routine is not done, the program will prompt the user to manually input calibration coefficients.
The following is a list of items needed in order to replicate this demo.
To obtain a most accurate results when taking measurements, process below should take into considerations:
We recommend not opening the project directly, but rather import it into CCES and make a local copy in your workspace.
The source code and include files of the ADuCM360_demo_cn0409 can be found on Github:
CrossCore Embedded Studio Application Source Code:
AduCM360_demo_cn0409 at Github
For more information on importing, debugging, or other tools related questions, please see the tools user guide.
Following is the UART configuration.
Select COM Port Baud rate: 9600 Data: 8 bit Parity: none Start: 1 bit Stop: 2 bit Flow Control: none
The official tool we promote for use with the EVAL-ADICUP360 is CrossCore Embedded Studio. For more information on downloading the tools and a quick start guide on how to use the tool basics, please check out the Tools Overview page.
For more detailed instructions on importing this application/demo example into the CrossCore Embedded Studios tools, please view our How to import existing projects into your workspace section.
For more detailed instructions on importing this application/demo example into the CrossCore Embedded Studios tools, please view our How to configure the debug session section.
The ADuCM360_demo_cn0409 is a C++ project that uses ADuCM36x C/C++ Project structure.
This project contains: system initialization part, setting system clock, enabling clock for peripherals; i2c interface, UART via P0.6/P0.7; UART read/write functions; Memory read/write functions; turbidity calculations;
In the src and include folders you will find the source and header files related to CN0409 software application. The Communication.cpp/h files contain UART and I2C specific data, meanwhile the CN0409.cpp/h files contain the calculation part and Flash.cpp/h provide memory management. .
End of Document