This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0409 [05 Jul 2018 10:32] – Mircea Caprioru | resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0409 [14 Mar 2021 10:09] (current) – [Obtaining the Source Code] adding in .Bin file Zuedmar Arceo | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Turbidity Measurement Demo (with EVAL-CN0409-ARDZ) ====== | ====== Turbidity Measurement Demo (with EVAL-CN0409-ARDZ) ====== | ||
- | The **EVAL-CN0409-ARDZ** shield is a low to high level water turbidity measurement system in combination with the EVAL-**ADICUP360**. It uses the **ADPD105' | + | ===== General description ===== |
+ | The **EVAL-CN0409-ARDZ** shield is a low to high level water turbidity measurement system in combination with the **EVAL-ADICUP360**. It uses the **ADPD105' | ||
{{ : | {{ : | ||
- | ===== General description | + | ===== Setting up the hardware |
- | The **ADuCM360_demo_cn0409** | + | |
+ | - To program the base board, set the jumpers/ | ||
+ | - Connect the **EVAL-CN0409-ARDZ** to the Arduino connectors **P2, P5, P6, P7, P8** of the **EVAL-ADICUP360** board. | ||
+ | - Plug in the USB cable from the PC to the EVAL-ADICUP360 base board via the Debug USB.(P14) | ||
==== Calibration procedure ==== | ==== Calibration procedure ==== | ||
Line 10: | Line 14: | ||
The user has the option to modify the solutions that are used for calibrating the device. | The user has the option to modify the solutions that are used for calibrating the device. | ||
- | {{ : | + | {{ : |
+ | <WRAP center round info 60%> | ||
+ | These values can be edited in **CN0409.h** file inside the include folder within the project structure. | ||
+ | </ | ||
+ | After the calibration sequence is done at least once, the calibration coefficients are saved in the controller flash memory and will be used the next time when a calibration is not done. The calibration can be repeated as desired. If the program is run for the first time and a calibration routine is not done, the program will prompt the user to manually input calibration coefficients. | ||
===== Demo Requirements ===== | ===== Demo Requirements ===== | ||
Line 58: | Line 66: | ||
{{: | {{: | ||
- | ===== Obtaining the source code ===== | + | ===== Obtaining the Source Code ===== |
- | We recommend not opening | + | |
+ | There are two basic ways to program | ||
+ | - Dragging and Dropping the .Bin to the MBED drive | ||
+ | - Building, Compiling, and Debugging using CCES | ||
+ | |||
+ | Using the drag and drop method, the software is going to be a version that Analog Devices creates for testing and evaluation purposes. This is the EASIEST way to get started with the reference design. | ||
+ | |||
+ | Importing the project into CrossCore is going to allow you to change parameters and customize the software to fit your needs, but will be a bit more advanced and will require you to download the CrossCore toolchain. | ||
+ | |||
+ | The software for the **ADuCM360_demo_cn0409** demo can be found here: | ||
- | The source code and include files of the ADuCM360_demo_cn0409 can be found on Github: | ||
<WRAP round 80% download> | <WRAP round 80% download> | ||
- | \\ | + | Prebuilt CN0409 Bin File |
- | CrossCore Embedded Studio Application Source Code: | + | * [[https:// |
- | \\ | + | Complete CN0409 Source Files |
- | \\ | + | |
- | [[https:// | + | |
- | </ | + | |
+ | </ | ||
<WRAP center round info 80%> | <WRAP center round info 80%> | ||
- | For more information on importing, debugging, or other tools related questions, please see the [[https:// | + | For more information on importing, debugging, or other tools related questions, please see the [[/ |
</ | </ | ||