This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0409 [08 Feb 2019 22:25] – Add ADICUP360 switch configuration Mark Thoren | resources:eval:user-guides:eval-adicup360:reference_designs:demo_cn0409 [20 Feb 2019 22:11] – added serial terminal from other source page Brandon Bushey | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== Turbidity Measurement Demo (with EVAL-CN0409-ARDZ) ====== | ====== Turbidity Measurement Demo (with EVAL-CN0409-ARDZ) ====== | ||
- | The **EVAL-CN0409-ARDZ** shield is a low to high level water turbidity measurement system in combination with the EVAL-**ADICUP360**. It uses the **ADPD105' | + | ===== General description ===== |
+ | The **EVAL-CN0409-ARDZ** shield is a low to high level water turbidity measurement system in combination with the **EVAL-ADICUP360**. It uses the **ADPD105' | ||
{{ : | {{ : | ||
- | |||
- | ===== General description ===== | ||
- | The **ADuCM360_demo_cn0409** | ||
===== Setting up the hardware ===== | ===== Setting up the hardware ===== | ||
Line 16: | Line 14: | ||
The user has the option to modify the solutions that are used for calibrating the device. | The user has the option to modify the solutions that are used for calibrating the device. | ||
- | {{ : | + | {{ : |
+ | <WRAP center round info 60%> | ||
+ | These values can be edited in **CN0409.h** file inside the include folder within the project structure. | ||
+ | </ | ||
+ | After the calibration sequence is done at least once, the calibration coefficients are saved in the controller flash memory and will be used the next time when a calibration is not done. The calibration can be repeated as desired. If the program is run for the first time and a calibration routine is not done, the program will prompt the user to manually input calibration coefficients. | ||
===== Demo Requirements ===== | ===== Demo Requirements ===== | ||
Line 50: | Line 52: | ||
- If possible, use one properly indexed test vial. | - If possible, use one properly indexed test vial. | ||
< | < | ||
+ | |||
+ | ===== Serial Terminal Setup ===== | ||
+ | |||
+ | {{page>/ | ||
===== Measurement Procedure ===== | ===== Measurement Procedure ===== |